2024-06-20 6:13 AM
I wanted to use the ioc and all the code from a project into another project. So, I copied the project and pasted in a workspace, then renamed the project, but ioc is not changed. So while opening, I get error message
Invalid Input: Must be project's active .ioc file.
Project's 'board_HW_Test' active one is 'board_HW_Test.ioc' file
Do I need to rename only the ioc or any other changes without loosing the data.
Solved! Go to Solution.
2024-06-20 10:32 AM
I just renamed the ioc file
2024-06-20 8:43 AM
The project name must match the name that is also stored in the IOC under
Normally you should not change the IOC, but if you have a backup copy, you can open it now with a text editor (e.g. Notepad++) and change these strings to the new name.
Hope that helps?
Good luck!
/Regards
2024-06-20 9:35 AM
But why does cubeIDE does not make that change when I use the option to rename project?
2024-06-20 10:32 AM
I just renamed the ioc file