cancel
Showing results for 
Search instead for 
Did you mean: 

Random source files opening in CubeIDE when downloading firmware

Ricko
Senior II

Hi,

every time I download the code from CubeIDE into the micro, a seemingly random file (every time a different one) opens up in the editor. More specifically it opens in the split editor area that is active when I press Run (i.e. left window or right window in the editor screenshot below).

Furthermore it opens only system/library source and header files like stm32l4xx_ll_adc.h, stm32l4xx_hal_tim_ex.c and stm32l4xx_hal_gpio.c and not the source files I created.

Any idea why and how to prevent it from doing that?

Thank you

Ricko_0-1726082073502.png

 

1 REPLY 1
padawan
Senior

Hi Ricko,

this is an old issue.

https://community.st.com/t5/stm32cubeide-mcus/jumping-to-random-file-after-pressing-run-button/m-p/246693

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-14-0-gt-old-issue/m-p/612850

They tagged it as "solved" by opening a ticket.

They will fix it "asap" since over 4 years

padawan