2023-11-15 09:47 PM
@Semer CHERNI
plz help with this problem.
Board : STM32H745I - DISCO
Cubeide : v.1.13.2
TouchGFX : v4.22.1 Designer
STM32H745I - DISCO as it is dual core m4 and m7
1st i did build and debugging for m4 processor. It is successful.
2nly done with building for m7 processor.It is successful
But while debugging the m7 i am facing following issue ??????
Solved! Go to Solution.
2023-11-16 01:31 AM
Hello,
First let me thank you for posting.
Could you please share the debug configuration for both project with the Debugger and Startup view.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-16 01:31 AM
Hello,
First let me thank you for posting.
Could you please share the debug configuration for both project with the Debugger and Startup view.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-16 01:39 AM
Thanks sir
I found one of the solution in which external loader setting was done.
i did the same and issue is solved