2024-06-06 3:17 PM
Keil (among others) allows the choice of whether to do a full or partial erase before programming:
Is it possible to do that in STM32CubeIDE ?
If so, how ?
Solved! Go to Solution.
2024-07-05 8:18 AM
If your requirements are to specifically do this through existing options provided by the IDE - I can't help.
But CubeProgrammerCLT does give you fine control about what to erase and what to write:
CMD> STM32_Programmer_CLI.exe
Available commands for STM32 MCU:
-e, --erase : Erase memory pages/sectors devices:
Not supported for STM32MP
[all] : Erase all sectors
[<sectorsCodes>] : Erase the specified sectors identified by sectors
codes. ex: 0, 1, 2 to erase sectors 0, 1 and 2
for EEPROM : ed1 & ed2
[<[start end]>] : Erase the specified sectors starting from
start code to end code, ex: -e [5 10]
-w, --write
-d, --download : Download the content of a file into device memory
<file_path> : File path name to be downloaded: (bin, hex, srec, s19
elf, stm32 or tsv file)
[<address>] : Start address of download
-w64 : Write a 64-bits data into device memory
<address> : Start address of download
<64-bit_data> : 64-bit data to be downloaded
values should not be separated by space
-w32 : Write a 32-bits data into device memory
<address> : Start address of download
<32-bit_data> : 32-bit data to be downloaded
values should be separated by spaceSo with some tinkering, you could probably get what you want by that route.
Alternatively, the open-source flashrom project supports stlinkv3, so you could also hack a custom command into that.
Once you have a script/program that does what you want, you should be able to plug that into your IDE flow so that programming is done using that tool. Worst case, jerryrig a file-watcher util to launch your download script whenever it detects a change in the compiled binary, and tell your IDE not to download when you start a debug session.
2024-07-05 8:42 AM - edited 2024-07-05 8:50 AM
Then somethink in your code place some on end of flash = linker erase all flash.
Show log from GDB flashing code . Or maybe you dont use ST GDB for load, how it does JLink and other probes maybe differ
2024-07-05 9:20 AM
@MM..1 wrote:Show log from GDB flashing code .
Is that log saved somewhere?
2024-07-05 9:23 AM
@Andrew Neil wrote: Using Flash for non-volatile data storage (EEPROM emulation) - where you want to be able to down load new firmware without erasing the NV data.
Have you tried modifying the linker script to exclude a portion of flash address space, and allocating that range to a new custom section dedicated to NV storage?
2024-07-05 9:33 AM - edited 2024-07-05 9:34 AM
So far, I've just used it as-is from the App Note - which doesn't modify the linker script; just uses "magic number" addresses for NV storage:
#define NB_OF_PAGES 2
/* Pages 0 and 1 base and end addresses */
#define PAGE0_BASE_ADDRESS ((uint32_t)(EEPROM_START_ADDRESS + 0x0000))
#define PAGE0_END_ADDRESS ((uint32_t)(EEPROM_START_ADDRESS + (PAGE_SIZE - 1)))
#define PAGE1_BASE_ADDRESS ((uint32_t)(EEPROM_START_ADDRESS + 0x0400))
#define PAGE1_END_ADDRESS ((uint32_t)(EEPROM_START_ADDRESS + (2 * PAGE_SIZE - 1)))uint16_t EE_Init(void)
{
uint16_t PageStatus0 = 6, PageStatus1 = 6;
uint16_t EepromStatus = 0;
uint16_t FlashStatus;
/* Get Page0 status */
PageStatus0 = (*(__IO uint16_t*)PAGE0_BASE_ADDRESS);
/* Get Page1 status */
PageStatus1 = (*(__IO uint16_t*)PAGE1_BASE_ADDRESS);
So the tools would have no knowledge that the space was being used for anything?
(this does strike me as a Bad Idea, but I hadn't got as far as addressing that yet)
Perhaps @Semer CHERNI (or someone else from ST) could confirm what should be the behaviour of STM32CubeIDE here - should it be erasing the whole chip, or should just erase enough to cover the code being loaded?
Off for the weekend now ...
2024-07-05 10:37 AM
> So the tools would have no knowledge that the space was being used for anything?
At least the GNU tools have no idea. IAR toolchain seems to be smarter in interop between compiler and linker. (But I don't use it recently, as the customers migrate to "free cheese").
2024-09-26 7:22 AM
@MM..1 wrote:No i repeat erased is all you config in linker file. Normal only used parts..
The default Linker file specifies the whole of Flash:
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 8K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 64K
}
So, if I were to make that just 62K, it would leave 2K untouched at the end of the Flash?
2024-09-26 9:02 AM
This in linker file only declare areas, not erasing. And yes for eeprom emulating is good practice reduce LENGTH.
I use IDE long time and never have trouble with erase all sectors. Always is erased only required. Ofcourse using STLINK GDB Server for load
2024-09-26 9:14 AM
@MM..1 wrote:This in linker file only declare areas, not erasing.
So what part of the linker file were you referring to when you said
@MM..1 wrote:i repeat erased is all you config in linker file
2024-10-23 4:02 AM
@MM..1 wrote:IDE work this way erase only code linker parts. I use this daily
Yes, in fact it does!
@Andrew Neil wrote:Not in my experience - it erased everything.
It seems I was mistaken: Keil defaults to the full-chip erase, but STM32CubeIDE only erases as much Flash as needed.