2019-05-20 09:55 PM
Hello all,
after trying several attemts and hint's i am still confused what's wrong with my configuration or Board.
Currently no slave is conected, i just wan't do display at least clock ans MOSI
Please have a look at the attached STM32Cube IDE Projekt.
Let me know, where i have made the mistakes.
Thanks in advance
Marc
2019-05-21 01:35 PM
I looked in the Cube file.
NSSP mode ? Why do you want to pulse the nSS pin ?
nSS functionality in STM doesn't work very well, so we dont use it
We use the software nSS signal.
a Prescaler of 2 is too small, 54MHz seems too fast.
there is no software in that zip file.
no main.c ??
2019-05-22 02:09 AM
2019-05-22 03:01 AM
you would usually spi_Init before while(1){};
you only need to initialize once.
also you should move the deinit to below while(1){}
then you would get a scope to look at the wires, are you doing that ?
I dont see the nSS being software driven ...
2019-05-22 04:06 AM
Hello TJ,
i am currently at work, i will make the changes when i am back at home 😉
I will test using this: http://www.zeroplus.com.tw/logic-analyzer_en/products.php
But i can take a acope for additional reference to.
I will report the results after that
2019-05-22 09:01 PM
Hi,
no changes at all: No output at the port pins.
SPI Result codes in code looks ok during Debug, but mo output.
To shorten this:
Does someone have a working SPI example for me, that was used / created by yourself on exactly this board.
And is it possible to provide this for reference.
Actually i don't have at least one reliably reference spI Project for this board.
Or:
Can someone simply test (no theretical discussion) my project on his nucleo board and agree that he has output on Pins or not.
Thanks Marc