2024-07-16 4:34 AM
Hello,
I have a problem that I haven't been able to solve for a few days...
I have a project with a NUCLEO-F767ZI that was working a few days ago and now I can't connect to its ST-Link probe.
I instantly get the message: “No ST-LINK detected!Please connect ST-LINK and restart the debug session.”
I tested the following points:
I don't know what to test, if you have any clues to help me, I'd love to hear from you.
Thanks a lot!
2024-07-16 4:37 AM
@Armageddon wrote:
- I can connect and program with STM32CubeProgrammer
Do you disconnect (maybe also close) the Cube Programmer before trying with the IDE?
2024-07-16 4:41 AM
Yes, I disconnect and close, I didn't have STM32CubeProgrammer before.
I installed it just to ckeck if I could connect to my board.
2024-07-16 4:59 AM
Please post the full Console output for when you try to start a debug session.
Also screenshot(s) of any error pop-up(s)
2024-07-16 5:06 AM - edited 2024-07-16 5:07 AM
My Debugger console is empty.
When I click on the debug icon, I just have the following windows who pop instantly.
The last message of my console is just "Build Finished. 0 errors, 0 warnings."