2020-10-28 03:03 PM
Have installed STM32CubeIDE on my Debian Linux system.
Following the QuickStart Guide, I try: File > New > STM32 Project
and it thinks about it and the gives me:-
What did I forget to do and where does it tell me to do it?
Solved! Go to Solution.
2020-10-31 03:05 AM
Sorted!
A bit more searching with a modified question lead me to this:-
https://community.st.com/s/question/0D50X0000C8elXsSQI/target-selection-window-is-empty
So, Wayland strikes again! I have now disabled Wayland and STM32CubeIde is working as it should :smiling_face_with_smiling_eyes:
2020-10-28 03:44 PM
That's the page to select a chip, which you need to do. Maybe you need to resize the window or something to see the options.
2020-10-29 01:26 AM
Sorry, I cropped the screenshot to just show the message.
This is the sequence of events after File > New > STM32 Project:
First it appears to be doing something ...
Then the Target Selection windows opens, empty ...
I have checked out Installation to Project instructions and walk-through videos and they all show this last window fully populated.
Luckily, I haven't invested in any hardware yet ;)
Also noticed and it may be related.
If I select Help > Check for Target Selector Device Database Updates,
I get this:
Which just sits there until I get bored and close it.
2020-10-29 07:41 AM
You do need to be connected to the internet as downloads some packages, at least the first time you run it. If you're behind a proxy, it probably won't work out of the box. If that's not it, I'm not sure.
You could try standalone STM32CubeMX to see if it has the same issue.
2020-10-29 11:29 AM
The internet connection is permanent and the other software update and install functions from Help all work.
I checked my firewall and it is not blocking any outgoing connection attempts.
As for standalone STM32CubeMX:
Downloaded and installed it and it does not show the problem, neither does it cure it in STM32CubeIDE.
If it actually works, I went no further than checking the Target Selector, then I suppose it could be a workaround albeit rather clumsy ...
more of a Disintegrated Development Environment.
Would be nice to get it working properly :smirking_face:
2020-10-31 03:05 AM
Sorted!
A bit more searching with a modified question lead me to this:-
https://community.st.com/s/question/0D50X0000C8elXsSQI/target-selection-window-is-empty
So, Wayland strikes again! I have now disabled Wayland and STM32CubeIde is working as it should :smiling_face_with_smiling_eyes:
2020-10-31 03:14 AM
Sounds more like Eclipse strikes again... :)
2020-10-31 03:42 AM
That is a whole different argument :D
But I find it easier to disable Wayland than rewrite Eclipse (and Synaptic) to be compatible (and probably others as well ...) :smirking_face: