2024-05-14 10:54 PM
I cannot login in the STM32CubeIDE V1.15.1, it keeps falling, I have a plain private internet connection without any additional firewall than the one there is on my computer. I do not use vpn.
Everything else Works fine on the internet
i have also tried to disable my firewall, still no luck, Have also tried hotspot on my phone, no difference
I have tried all three network settings under the preferences.
I can login in the browser, but I cannot download the software for reinstall, everytime it keeps prompting me for login into stm again, even that I already is logged in.
I have tried to restart my computer several time.
On my computer at my workspace it works at it should.
Solved! Go to Solution.
2024-06-17 01:00 PM
Dear @Kvang ,
Original issue solved by 17th May 2024 The CubeMX/CubeIDE login issue is resolved - STMicroelectronics Community.
Cheers,
STOne-32.
2024-05-15 06:23 AM
Need to login to update the HAL libraries...
Any minute now...
And... fail. Again.
2024-05-15 07:30 AM
Hi @Kvang
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2024-05-15 05:31 PM
I'm also having the same issue.
2024-05-15 08:57 PM
I am also completely out of commision due to this error.
2024-05-16 01:35 AM
With respect, there are more of us than just Kvang with this problem. This is impeding our ability to do any work here. Thanks.
2024-05-16 03:24 AM
same issue for 2 days now, for un unnecesssary lock. why having to log Cube ??? If it cannot log, let it run.
2024-05-16 06:56 AM - edited 2024-05-16 10:54 AM
I'm still down... I can log in through the web site, but the CubeIDE (1.15.1) will not log in. It hangs and says the network is down. I have no proxy, VPN, or firewall blocks. I am working on a new design and can't generate code from the ioc file if not logged in. I would strongly recommend making login optional for critical tasks and just keep retrying in the background.
NOTE: I had another system that was logging in on its own at startup just fine. I stupily logged out to see if the problem was machine specific and now that system won't log in either.
UPDATE: Can confirm the error occurs on both Linux and Windows versions. It seems to be on the Server side.
2024-05-16 11:39 AM
Same issue here.
Huge bummer having just picked up an STM board for the first time...
2024-05-16 11:47 AM
workaround: install CubeIDE 1.12.1
It has no login functionnality and use latest packages.
if Cube MX is not conveniant, you can open your IOC file in a text writer and change this line
MxCube.Version=6.8.1
to your version.