2022-03-08 02:39 PM
I get a multiple definition error for every variable declared inside a .h file after updating from CubeIDe 1.8.0 to 1.9.0. The previous CubeMX version was 6.3.0 and now it is 6.5.0. Before updating there would be no errors while building the code. The .h file has the header guards generated by the IDE. Is there any way to fix this?
Solved! Go to Solution.
2022-03-09 02:14 AM
See https://gcc.gnu.org/gcc-10/porting_to.html
"A common mistake in C is omitting extern when declaring a global variable in a header file. If the header is included by several files it results in multiple definitions of the same variable. In previous GCC versions this error is ignored. GCC 10 defaults to -fno-common, which means a linker error will now be reported. To fix this, use extern in header files when declaring global variables, and ensure each global is defined in exactly one C file. If tentative definitions of particular variables need to be placed in a common block, __attribute__((__common__)) can be used to force that behavior even in code compiled without -fcommon. As a workaround, legacy C code where all tentative definitions should be placed into a common block can be compiled with -fcommon"
.
2022-03-09 02:14 AM
See https://gcc.gnu.org/gcc-10/porting_to.html
"A common mistake in C is omitting extern when declaring a global variable in a header file. If the header is included by several files it results in multiple definitions of the same variable. In previous GCC versions this error is ignored. GCC 10 defaults to -fno-common, which means a linker error will now be reported. To fix this, use extern in header files when declaring global variables, and ensure each global is defined in exactly one C file. If tentative definitions of particular variables need to be placed in a common block, __attribute__((__common__)) can be used to force that behavior even in code compiled without -fcommon. As a workaround, legacy C code where all tentative definitions should be placed into a common block can be compiled with -fcommon"
.
2022-03-09 07:41 AM
@Rodolfo_Rodrigues, do you find these issues in CubeMX generated code?
If, so please let us know Cube package, revision, files, lines, ...
Then I can file some tickets and dispatch to the right teams for a first analysis of the scope.
2022-03-09 07:57 AM
No, it only happened with the code i've written. After applying what @CButz.1 said in his comment the errors were gone.
2022-03-11 07:10 AM
I have this too with all my projects. I returned to v.1.8.0. for the moment
I have one .h-file that is included from several .C-files.
Therefor I put this on the beginning of each .h-file:
#ifndef PMT_H_
#define PMT_H_ 1
// declarations come here
#endif /* PMT_H_ */
So, if this .h-file is included several times, the declarations are only done once: the first time it is included.
This worked before version 1.9.0, and not any longer with 1.9.0
Wouldnt there be a solution? Why is the if-statement not working?
2022-03-11 07:22 AM
the toolchain changed to gcc 10 and therefore tentative definitions in header files are no longer ignored.
You should not define variables in headers, but rather use extern in header files and define it in one source file. This has always been a error, but was ignored in gcc 9. So to fix this either use -fcommon
to compile or the better solution is to declare the variables in the header as "extern" and define them in one source file. Heres the link to the GNU GCC 10 source:
https://gcc.gnu.org/gcc-10/porting_to.html
As this problematic isnt bound to cubeide but rather C and gcc 10 here is a external link that maybe helps:
https://stackoverflow.com/questions/1164167/variable-declaration-in-a-header-file
2022-03-14 02:48 AM
Thanks for the clarification!
2022-03-29 04:06 PM
Apparently this is some new bug. had it just after updating the project to the new version.
Solution that worked for me: open project properties -> settings, under MCU GCC Compiler select Miscellaneous. Click add flag -fcommon
2022-06-22 02:58 PM
Thanks! It works!
2022-07-08 02:12 PM
Thanks a lot.