User Activity

We are currently trying to build a external loader for our application.Our System consists of a STM32H743 and a STM32F427ZIT.For the initial upload of the firmware the DFU interface of the H7 should be used and via a external loader application loade...
Hi there,I am currently trying to get TouchGFX working on the U575I-Eval Board.Is there a project to start from?I made a new project with components initialised and TouchGFX activated.What do I need to activate too?Do I need the hx8347i driver? (from...
So i need to setup a tcp server on the f4, easy as there are examples using netx. But i am forced to use HAL 1.27 which is in no way compatible with the old eth drivers, i dont need the performance win of the new ETH HAL, but whenever i try to change...
Is the STM32F43x under any import/export regulations, if you want to export a product with F43x to china? Because for example china has theyre import and export list for crypto devices. Or in regard of Wassenaar Arrangement? Even tho our product does...
I want to make a Filesystem with FileX and use the usbx device storage class to get access to the files. I successfully created a FileX filesystem on ram. I found the examples Ux_Device_MSC, this uses the sd card for the file system.In ux_device_msc....
Kudos given to