2025-01-22 5:29 AM - edited 2025-01-22 5:38 AM
Hi,
It seems the X-CUBE-AZRTOS-F7 1.1.0 is based on ThreadX 6.1.7. But after select 'Enable BASEPRI support', it missed several files which exist in the official 6.1.7 release, they are:
tx_thread_interrupt_disable.S and _tx_thread_interrupt_restore.S.
Thanks.
'
Solved! Go to Solution.
2025-01-28 2:38 AM - edited 2025-01-29 8:06 AM
Hello @diverger ,
Thank you for reporting this issue:
Missing declaration of tx_thread_interrupt_restore.s and tx_thread_interrupt_disable.s in STMicroelectronics
X-CUBE-AZRTOS-F7.1.1.0_Configs.xml for the CM7 GNU.
I am escalating an internal ticket to the concerned team (ticket number:201630).
Thanks.
Mahmoud
2025-01-22 6:06 AM
Hello @diverger ,
First let me thank you for posting.
I have created a project with STM32F722ICK6 and I have installed and enabled X-CUBE-AZRTOS-F7.
tx_thread_interrupt_disable.S and _tx_thread_interrupt_restore.S are well generated.
Thanks.
Mahmoud
2025-01-24 6:26 PM - edited 2025-01-24 6:26 PM
Hi,
It's weird that your MCU is a F7 based on cortex-m7, but it shows 'cortex-m33' in the picture. In my case, I use STM32F769.
Please check it.
Thanks.
2025-01-27 7:37 AM
Hello @diverger ,
Further to your comment, I am using STM32CubeMX 6.13 and ThreadX version: 6.1.10 not 6.1.7.
Thanks.
Mahmoud
2025-01-28 2:38 AM - edited 2025-01-29 8:06 AM
Hello @diverger ,
Thank you for reporting this issue:
Missing declaration of tx_thread_interrupt_restore.s and tx_thread_interrupt_disable.s in STMicroelectronics
X-CUBE-AZRTOS-F7.1.1.0_Configs.xml for the CM7 GNU.
I am escalating an internal ticket to the concerned team (ticket number:201630).
Thanks.
Mahmoud