2025-01-22 05:29 AM - edited 2025-01-22 05:38 AM
Hi,
It seems the X-CUBE-AZRTOS-F7 1.1.0 is based on ThreadX 6.1.7. But after select 'Enable BASEPRI support', it missed several files which exist in the official 6.1.7 release, they are:
tx_thread_interrupt_disable.S and _tx_thread_interrupt_restore.S.
Thanks.
'
2025-01-22 06:06 AM
Hello @diverger ,
First let me thank you for posting.
I have created a project with STM32F722ICK6 and I have installed and enabled X-CUBE-AZRTOS-F7.
tx_thread_interrupt_disable.S and _tx_thread_interrupt_restore.S are well generated.
Thanks.
Mahmoud