cancel
Showing results for 
Search instead for 
Did you mean: 

MCU: STM32F030K6T. remape vector table scince the register VTOR is not availbe on this MCU.

MSadk.2
Associate II

MCU: STM32F030K6T. I have the problem remape vector table scince the register VTOR is not availbe on this MCU. I would like to ask how i can remape the vector table on this MCU to one of my application address 0x08001000 or 0x08004800. I have been doing this procces on STM32G030F6P and it was working fine. This is the code for G Type MCU int main(void){

if (IMAGE_1 == *((__IO uint32_t*) SRAM_SELECT_ADDRESS)) {

uint32_t addressImage1 = imageAddress(CONFIG_ADDRESS, IMAGE_1);

SCB->VTOR = addressImage1 + 4;

}

if (IMAGE_2 == *((__IO uint32_t*) SRAM_SELECT_ADDRESS)) {

uint32_t addressImage2 = imageAddress(CONFIG_ADDRESS, IMAGE_2);

SCB->VTOR = addressImage2 + 4;

}

 /* MCU Configuration--------------------------------------------------------*/

platform_start();

HAL_UART_Receive_IT(&huart2, uartRxbuffer, sizeof(uartRxbuffer));

while(1){

// waiting for an interrupt.

}

}

Thanks in advance for your help

This discussion is locked. Please start a new topic to ask your question.
18 REPLIES 18
gbm
Principal

You can't.

You can, however, do something different instead: fiddle a little with the linker script to put the vectors at the start of RAM, then put RAM at address 0.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
MSadk.2
Associate II

thank you

Wijeden RHIMI
ST Employee

Hello@MSadk.2,

I wonder ask you if your issue was resolved or you are stilling blocked :smirking_face:?

I wait your reply.

Best regards,

Wijeden,

MSadk.2
Associate II

thanks for your quastion!

actually i needed to know if it is possible to go similar to STM32G030F6P.

if you have different solution, it would be nice to recommended.

Wijeden RHIMI
ST Employee

Hi again @MSadk.2,

Please check which board exactly you are working with .Because, it seems that is a typing error existing here  'STM32030K6T ' and also if you are switching to use 'STM32G030F6P' board?

I wait your answer.

Wijeden,

MSadk.2
Associate II

yes i forgot the F STM32F030K6T

Wijeden RHIMI
ST Employee

Ok good so you want to use STM32F030K6T board ?

MSadk.2
Associate II

yes thanks for your answer

Wijeden RHIMI
ST Employee

Hi again,

Could you please provide a complete project to help us reproduce your issue and further analyze it .

Wijeden,