Skip to main content
Associate
January 13, 2024
Question

Loading problem with STM32CubIDE_1.14.0

  • January 13, 2024
  • 7 replies
  • 1985 views

Hi,

I'm trying to get running with a STM32F446. I'm using a Nucleo 64 board for now. I've installed CubeIDE on a new computer running Windows 10 and I get Make error 2 and the messages that it can't find gcc and g++. It seems to be a problem with paths. Could it be looking for some files from a previous version which do not exist on my new computer? I believe the paths and the missing files did not get installed with 1.14.0. What is the path and where do I get the files and where do I put them?

This topic has been closed for replies.

7 replies

TDK
January 13, 2024

Perhaps create a new project, ensure it builds correctly, and copy your files over to that new project. The toolchain may have changed between versions.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
January 18, 2024

Hi TDK,

I have tried that. The problems don't seem to be at the project level, but probably at the system level. The toolchain files seem not to exist. I have tried uninstalling  STM32CubeIDE and reinstalling it with the same result.

Ron

Pavel A.
January 18, 2024

Same issue? https://community.st.com/t5/stm32cubeide-mcus/cannot-build-imported-stm32-project/td-p/628123

In the project settings add this pre-build command:  echo "$$PATH". What will it print?

Associate
January 19, 2024

Hi Pavel,

Under Run/Debug Settings, I was unable to edit anything. Is there another thing I can try? I have done at least a hundred TI MSP430 and TMS4C projects (Code Composer is another Elipse based IDE), and I have never run into this sort of problem.

Ron

Associate
January 19, 2024

Hi Pavel,

I was able to run the path command from build preprocessor setting and got back ' '.

Ron