2024-01-13 10:51 AM
Hi,
I'm trying to get running with a STM32F446. I'm using a Nucleo 64 board for now. I've installed CubeIDE on a new computer running Windows 10 and I get Make error 2 and the messages that it can't find gcc and g++. It seems to be a problem with paths. Could it be looking for some files from a previous version which do not exist on my new computer? I believe the paths and the missing files did not get installed with 1.14.0. What is the path and where do I get the files and where do I put them?
2024-01-13 10:55 AM
Perhaps create a new project, ensure it builds correctly, and copy your files over to that new project. The toolchain may have changed between versions.
2024-01-17 5:56 PM
Hi TDK,
I have tried that. The problems don't seem to be at the project level, but probably at the system level. The toolchain files seem not to exist. I have tried uninstalling STM32CubeIDE and reinstalling it with the same result.
Ron
2024-01-17 6:27 PM - edited 2024-01-17 6:41 PM
Same issue? https://community.st.com/t5/stm32cubeide-mcus/cannot-build-imported-stm32-project/td-p/628123
In the project settings add this pre-build command: echo "$$PATH". What will it print?
2024-01-19 8:13 AM
Hi Pavel,
Under Run/Debug Settings, I was unable to edit anything. Is there another thing I can try? I have done at least a hundred TI MSP430 and TMS4C projects (Code Composer is another Elipse based IDE), and I have never run into this sort of problem.
Ron
2024-01-19 8:19 AM
Hi Pavel,
I was able to run the path command from build preprocessor setting and got back ' '.
Ron
2024-01-19 8:26 AM
If no project builds successfully, either the STM32CubeIDE installation is bad, perhaps due to an overzealous virus scanner, or you're doing something very wrong. I would assume the former is more likely, but if you wanted to include some screenshots of a fresh CubeMX generated project trying to be built, with the relevant error messages shown, might be able to spot something.
2024-01-19 11:44 AM - edited 2024-01-19 11:47 AM
Strange...
Is this a company-owned PC? Any "security" software or security policy installed by the IT?