cancel
Showing results for 
Search instead for 
Did you mean: 

live expression values gets corrupted while debugging with stm32cube ide version 1.14.0

Gaurav_rajput
Associate II

in debugging mode the values of variables gets corrupted when I check in live expressions. Here corrupted means shows wrong values.

20 REPLIES 20

@Rim LANDOLSI wrote:

The issue has already been reported to STM32CubeIDE development team. An internal ticket ID 168019


See also ticket 175214:

https://community.st.com/t5/stm32cubeide-mcus/live-expressions-bug/m-p/647398/highlight/true#M24957

@Ghofrane GSOURI 

chaari
Associate II

I had the same problem.

I just deleted CubeIDE and reinstalled it again. It Works good.

Nevermind. The porblem occured again after the next Debug.

It works when you delete all Live Expressions and add them again after starting the debug and resume.

This is a significant issue that hasn't been given adequate priority. Despite being reported over a year ago, I am still encountering this problem while using Cube IDE 1.16.1. This issue is causing delays in the debugging process, which in turn hinders product development progress.

hi Rim

 

Is there any update available on this issue?

thanks

paul

+1 Please fix this issue.

Best Regards.

I am also experiencing this error in CubeIDE version 1.14.0. The live variable sometimes initialize to nonsensicaly high values and I have to stop the debug and start again or reset the board.

I have reported the issue on my current installation, which is 1.17.0, but I have decided to report it in this thread instead of opening a new one. It is noteworthy that this issue is not listed in the errata as having been fixed or as a known bug.

Perhaps @Rim LANDOLSI, you could consider adding it to the list to facilitate future resolution.

Best regards,

I am having this issue with 1.18.0 as well. Doesn't seem to be fixed yet.