cancel
Showing results for 
Search instead for 
Did you mean: 

Linux installation error

shri1
Associate II
d64.deb'
Note, selecting 'st-stlink-udev-rules' instead of './st-stlink-udev-rules-1.0.3-2-linux-all.deb'
Note, selecting 'st-stm32cubeide-1.15.1' instead of './st-stm32cubeide-1.15.1-21094-20240412-1041_amd64.deb'
Note, selecting 'segger-jlink-udev-rules' instead of './segger-jlink-udev-rules-7.94h-linux-all.deb'
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:

The following packages have unmet dependencies:
st-stm32cubeide-1.15.1 : Depends: libncurses5 but it is not installable
Depends: libpython2.7 but it is not installable
Depends: libwebkit2gtk-4.0-37 but it is not installable
E: Unable to correct problems, you have held broken packages.

 

Which STM32IDE we should download to fix this error

13 REPLIES 13

linux ubuntu 24LTS

i had downloaded 1.15 stm32idecube linux installer

shri1
Associate II

You posted this as a reply to the Posting Tips - it's not appropriate there, so merged here.

 

d64.deb'
Note, selecting 'st-stlink-udev-rules' instead of './st-stlink-udev-rules-1.0.3-2-linux-all.deb'
Note, selecting 'st-stm32cubeide-1.15.1' instead of './st-stm32cubeide-1.15.1-21094-20240412-1041_amd64.deb'
Note, selecting 'segger-jlink-udev-rules' instead of './segger-jlink-udev-rules-7.94h-linux-all.deb'
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:

The following packages have unmet dependencies:
st-stm32cubeide-1.15.1 : Depends: libncurses5 but it is not installable
Depends: libpython2.7 but it is not installable
Depends: libwebkit2gtk-4.0-37 but it is not installable
E: Unable to correct problems, you have held broken packages.

 

Which STM32IDE we should download to fix this error

 

my os is ubuntu 24lts

stm32cube ide linux installer

yeah i had tried that as well but was showing the same error


@shri1 wrote:

i had downloaded 1.15 stm32idecube linux installer


Which one?

There are three:

AndrewNeil_0-1727196772959.png

https://www.st.com/en/development-tools/stm32cubeide.html#get-software

 

generic linux installer second one

stm32cubeide_1.15.1_21094_2012_1041_amd64.deb_bundl

BarryWhit_0-1727212689016.png

 

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.