cancel
Showing results for 
Search instead for 
Did you mean: 

Issue in buliding project and firmware updation in STMCUBEIDE

Ramya_06
Associate

Not able to build project, because the build icon is not enabled in STMCUBEIDE and firmware is getting updated multiple times. 

2 REPLIES 2
Rim LANDOLSI
ST Employee

Hello @Ramya_06  and welcome to the community,

Could you make sure that the connection is well set up in Preferences->Firmware Updater to be able to download the firmware correctly?
Otherwise, could you manually generate the code from the ioc file?

Thanks,

Rim.

Ramya_06
Associate

Thankyou for responding.

The Connection is proper in firmware setup, even then the same dialog box pops in with i have attached below and this prevents to generate the code. Please provide the solution for this issue.

 

 

 

Regards,

RAMYA