2021-06-14 07:40 AM
Hi,
I have really hard time to develop an Hyperbus protocol application on NUCLEO-L4R5ZI-P, the instruction is sent but the data are sent in a non-periodic sequence and DQS doesn't rise at the good time.
Is there someone who has develop the most simple application of Hyperbus communication that he could share with me?
I have tried to understand the exemple provided in that following link without success.
Thank you in advance for your help,
Kind regards.
2021-06-14 08:48 PM
@AGEBE.1 , I have not really tried HyperRAM myself. But, it seems there are two reference projects regarding HyperRAM inside STM32H7 FW package which may be helpful:
Regards,
Ethan
2021-06-23 04:27 AM
Thanks but it didn't solved my problem....