關於底下四個warning:(.text._close_r+0xc):警告:_close 未实现,并且总是失败(.text._lseek_r+0x10):警告:_lseek 未实现,并且总是失败(.text._read_r+0x10):警告:_read 未实现,并且总是失败(.text._write_r+0x10):警告:_write 未实现,并且总是失败可以試著在如下圖所示的linker設定當中將System calls改為 "Do not use system calls from libr...
According to the known limitations in Release_Notes.html, generating FreeRTOS projects for STM32N6 by STM32CubeMX or STM32CubeIDE is not supported yet:The STM32N6 projects are not generated with STM32CubeMX tool. In the case of creating a project fro...
According to the NOTE in Section 3.2.13 (External loader command) in UM2237 (Rev 24), using external loader over bootloader interface is not supported:NOTE: This command (-el) is only supported with SWD/JTAG ports.
Hi Alex,I'm not a VENC expert. According to the name of the API, EncAsicGetMvOutput in encasiccontroller.c (inside STM32Cube_FW_N6_V1.0.0\Middlewares\Third_Party\VideoEncoder\source\common) looks like what you need:/*---------------------------------...