2024-02-26 4:31 AM
Hi. I have seen several tutorials and read in the forum how to include a library. But it does not work. Can someone help me please.
Solved! Go to Solution.
2024-03-04 8:01 AM
thanks!
2024-03-04 8:03 AM
I can't test the code right now. But thank you so much!
2024-03-04 9:21 AM - edited 2024-03-04 9:23 AM
On the distinction between source and binary:
Traditionally, "Library" was used to mean a pre-built binary library.
Nowadays, people also commonly speak of source-code libraries.
2024-03-04 11:02 AM
Thank you so much for your help. I really appreciate that. I'm used to using Arduino and I'm still learning to program with the STIde. So thank you so much.
2024-03-05 2:17 AM
You're welcome.
Yes, one of the things that the Arduino IDE "hides" from you is these details behind adding a library.
Note that there are Arduino cores for STM32s; eg,
https://github.com/stm32duino/Arduino_Core_STM32
https://www.arduino.cc/reference/en/libraries/stm32duino-examples/
So using STM32 doesn't necessarily preclude continuing to use the Arduino IDE...
@Giuseppe1 wrote:I'm still learning to program with the STIde.
Note that this is general to C (and C++) development - it's not just specific to STM32 or the STM32CubeIDE.
2024-03-05 4:42 AM
@Andrew Neil wrote:
@Giuseppe1 wrote:I'm still learning to program with the STIde.
Note that this is general to C (and C++) development - it's not just specific to STM32 or the STM32CubeIDE.
yeah yeah i know.
Thanks a lot again for your help.
2024-03-07 6:59 AM
i think that i did it. I imported the source and the header file. But now i have this error (at least it is yellow and not red).
2024-03-07 7:13 AM - edited 2024-03-07 7:13 AM
Please give some more context on how & where you get that.
Does the code now build successfully ?
2024-03-07 9:51 AM
I installed and imported the the source file(.c) and the header(.h) file. Then instead of the first error(top of the discussion) it gave me that "yellow" error instead of a "red" one. Do you think I should create a new post?
2024-03-07 10:00 AM
@Giuseppe1 wrote:Do you think I should create a new post?
If the code does now build, then you have fixed the original problem.
You've marked the original problem as 'Solved', so this would seem to be a new problem.
In your new thread, you can always give the link to this thread for context...