cancel
Showing results for 
Search instead for 
Did you mean: 

I have STM32F407 and RJ45 connector. Can anybody tell me which stm32 pin to connect which RJ45 pin, so that i can go ahead with the web server over Ethernet project,RJ45 connector has 8 pins

psain.1
Associate II

STM32 with RJ45

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief III

right. need interface chip. i would take a cheap module, like this:

https://de.aliexpress.com/item/1005004446133417.html

0693W00000aH4K3QAK.pngalready with rj45 ... 

to connect : gnd, vdd , and these 9 pins:

0693W00000aH4MYQA0.png

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

7 REPLIES 7
AScha.3
Chief III

which board ? selfmade STM32F407 ?

STM32F407 chip has RMII interface, not rj45.

If you feel a post has answered your question, please click "Accept as Solution".
psain.1
Associate II

Yes, self made

so with RMII, how would I access the server over my router which has 8 pin RJ45 sockets

Am I supposed to use third party interface chip

AScha.3
Chief III

right. need interface chip. i would take a cheap module, like this:

https://de.aliexpress.com/item/1005004446133417.html

0693W00000aH4K3QAK.pngalready with rj45 ... 

to connect : gnd, vdd , and these 9 pins:

0693W00000aH4MYQA0.png

If you feel a post has answered your question, please click "Accept as Solution".
psain.1
Associate II

Okays

thank you

Piranha
Chief II

So you made a board, but didn't put an Ethernet PHY and connector on it. Why?

Did not had enough knowledge to do so.

now i am making upgraded one.

Piranha
Chief II

In my world at least the basic research comes first and designing of a hardware after that. I guess it requires a doctor's degree to take a look at ST's and other boards, which have an Ethernet and other features one requires. Most likely you haven't found the AN4488 either...