2024-02-13 10:55 AM - edited 2024-02-13 10:56 AM
Hello,
I am using stm32F407VGT board and I am trying to receive data from a can analyzer with stm32 board. I transmit a data to stm32 boards but ı cant receive the messages. I can work on normal mode with two stm32 boards succesfully. The messages are received and transmitted. At the same time, I want to transmit data to can analyzer and I want to observe communication. I attached my main and interrupt source files and I am using USB-CAN analyzerV8 device. The can bps values are the same 500kbps. The modes are same as Normal Mode and I dont define a filter so ı can read every data that ı sent from can analyzer in live expression on debug screen.
Summarize,
All my purpose, I want to see data that ı sent from can analyzer in my live expression part. I am sending one message fisrtly so there is a one Id.
2024-02-14 08:29 AM
By the way, If my can transciever circuit mcp2551 is wrong, How can I communicate with two stm32 board ? Could you show me an example transciever circuit with MCP2551 ? I will use that
2024-02-14 08:37 AM
See this thread the picture shared by the community member on his first post.
2024-02-14 08:56 AM
Thank you
I changed the terminal resistor with 120ohm on my can circuit and It still doesnt work. I cant understand my boards can communicate but why the analyzer can't ? I attached my can transciever circuit . I changed 60 ohm with 120ohm
2024-02-14 09:03 AM - edited 2024-02-14 09:42 AM
It seems you used "Test circuit" description for your project while this is not the right config:
So is that possible to:
2024-02-14 09:53 AM
I tried but it still doesnt work
I attached my code again. I used callback funcitons this time.
My software purpose's is the received message writed in rcount variable and this data is 1 bit.
2024-02-14 02:28 PM
You should check for HAL status when HAL_CAN_Start, HAL_CAN_ActivateNotification and
In the Error_Handler you can turn on an LED to indicate any of those 3 calls did not return HAL_OK.
if (HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/*##-3- Start the CAN peripheral ###########################################*/
if (HAL_CAN_Start(&CanHandle) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
/*##-4- Activate CAN RX notification #######################################*/
if (HAL_CAN_ActivateNotification(&CanHandle, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
2024-02-14 02:38 PM
thank you for reply
I will try this codes but I have a question
If I change my can transciever IC MCP2551 with TJA1051, Can it be better?
Which can transciever IC do you suggest?
2024-02-15 12:45 AM
Hello,
If I want to suggest a transceiver, I would choose either a transceiver with 3.3V supply like the ones used on our boards Ex: SN65HVD230.
Or a transceiver having Vio pin like TJA1051T/3 or TJA51TK/3 versions.
The transceivers TJA1051 and TJA1051T/E versions are not suitable for you because VIHmin = 0.7xVCC = 3.5V (if VCC=5V). So TX pin needs at least 3.5V > STM32 IO voltage (@3.3V).
MCP2551 still not bad because VIHmin = 2V < 3.3V
2024-02-15 09:48 AM
Hello again,
I readjusted my mcp2551 can transciever circuit and my codes. I attached them. But It still doenst work guys. The prgoram is not getting in canrxfifo ınterrupt function or I cant transmit data to analyzer. Maybe, the analyzer sends hex codes not decimal so can I read hex code data in my live expression panel ? I mean, should I decode the data in my codes ?
2024-02-15 11:55 AM
Attach your project. Draw up a diagram on how you've connected the MCP2551 to the STM32. How you've connected the CAN analyzer to the MCP2551, including power supply, USB connector(s) and grounds.