cancel
Showing results for 
Search instead for 
Did you mean: 

I am migrating STM32L073RZTx project from IAR to STMcude IDE. following error is showing while compiling in STMcude "Cannot find the specified linker script. Check the linker settings in the build configuration". Can any one help me solve the issue?

RNd.1
Associate
 
2 REPLIES 2
Florent V
ST Employee

Hi,

Please check if the path to the linker file set in the build properties of your project matches with your need. As the following screenshot for example:

0693W00000QNy5VQAT.png 

Regards,

Florent

Semer CHERNI
ST Employee

Hello @RNd.1​ 

Did this proposition came to help?

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.