Hi HaLed,Yes it's possible. You can define your shortcut through:Windows => preferences => General => keysUse the filter to find the "restart command" and set the shortcut using the binding field. BR,Florent
Hi,Please check if the path to the linker file set in the build properties of your project matches with your need. As the following screenshot for example: Regards,Florent
Hi @KFeng.2 ,Indeed it is a known bug on MacOS.Waiting for a fix, there are 2 workarounds:Download the pack manually and install it using "From Local..." button from "Embedded Software Packages Manager" window. OrIf the project has been created thro...
Hi,Do you use the restart button (Menu: File -> Restart) to close/open the CubeIDE? Because just after the update if you still only use the restart button the splash field is not updated:But then as soon as you close the CubeIDE through red cross or ...