2023-09-14 01:07 AM
Solved! Go to Solution.
2023-09-14 01:33 AM
Hello @Dushyantsingh
You may take a look at the configuration of HSE bypass in this project.
Best regards.
II
2023-09-14 01:33 AM
Hello @Dushyantsingh
You may take a look at the configuration of HSE bypass in this project.
Best regards.
II
2023-09-14 01:42 AM - edited 2023-09-14 01:43 AM
@Dushyantsingh it looks like you are using the NUCLEO-F429ZI with Zephyr, right?
However, your settings are not plausible, because with HSE=8MHz and &pll {div-m = <15>; ...} you only get 533.333kHz. The PLLM output frequency must be at least 950kHz. The current values in &pll{} also result in only 12.8MHz instead of 48MHz at output Q of the main PLL. So you should check your settings again with the RM0090 or CubeMX or CubeIDE.
Regards
/Peter