2023-05-28 2:11 PM
Recurring Error Message in STM32CubeIDE When Running or Debugging a Project. It shows-
'Launching pain Debug' Has encountered a problem.
Error in final launch sequence:
Failed to execute MI command: load
C:\\Users\\USER\\STM32CubelDE\\workspace_1.12.1\\pain\\ Debug\\pain.elf
Error message from debugger back end:
Error finishing flash operation.
and also it showing
"Error in final launch sequence:
Failed to execute MI command:
load C:\\Users\\USER\\STM32CubeIDE\\workspace_1.12.1\\try\\Debug\\try.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\USER\\STM32CubeIDE\\workspace_1.12.1\\try\\Debug\\try.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\USER\\STM32CubeIDE\\workspace_1.12.1\\try\\Debug\\try.elf
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation"
How to solve this problem? We are using STM32 NUCLEO-F446RE Board
2023-05-29 3:20 AM
Hello @Efty
First let me thank you for posting.
Could you provide the entire debug log.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-08 4:47 PM - edited 2023-11-20 4:28 AM
@Efty any luck on figuring this out? Since about a few months ago, I haven't been able to debug through STM32CubeIDE either. I've tried STLink v2 clones as well as the official STLink v3 that all used to be able to debug and flash through the IDE. They both work through the STM32CubeProgrammer to flash firmware files.
@Semer CHERNI If @Efty 's issue is like mine, that is the full debug log.
2023-09-08 1:05 AM
Hi, I've got the same issue. Here's the error log that appears in the failure message:
Error in final launch sequence:
Failed to execute MI command:
load C:\\TouchGFXProjects\\MyApplication\\STM32CubeIDE\\Debug\\STM32U5A9J-DK.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\TouchGFXProjects\\MyApplication\\STM32CubeIDE\\Debug\\STM32U5A9J-DK.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\TouchGFXProjects\\MyApplication\\STM32CubeIDE\\Debug\\STM32U5A9J-DK.elf
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation
Here are the messages from the console:
STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------
Warning: The external loader file does not exist:
MX25LM51245G_STM32U599J-DK.stldr
Encountered Error when opening C:\ST\STM32CubeIDE_1.13.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.0.202305091550\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
2023-09-10 12:09 PM
I was trying to programmatically access the flash on an stm32f411re. I had similar problems when I tried to use the debugger. What fixed it for me was to go to
menu item Project : Properties : Run/Debug Settings.
Edit the launch configuration. Tab Debugger. Change the Reset type behaviour to None.
2023-09-30 1:37 AM
Changing Reset type to None does not work for STM32U5A9J-DK.
2024-01-04 6:19 PM
Hello @Efty
I've got the same issue, there is the anwser:
change rtconfig.h, adjust your board stack size. in addition, you can use rt-thread setting, adjust you main thread, system thread .., the stack is overflow or whatever, It works.
2024-01-23 12:06 AM
Hi @Spark_Mars
Could you explain more about this solution? Where can I get rtconfig.h or adjust my board stack size. I can not find them (I'm new for STM, please helps me). Thank you so much
2024-03-03 4:50 AM
Hi everyone!
For those dealing with the same problem.. Have you checked your BOOT0 pin (jumper)?
I had the same issue on a custom hardware (my first PCB design with an STM32) using an STM32H503 in an LQFP64 package. Maybe I misread the datasheet for what to do with the BOOT0 pin, but I only soldered in the pullup resistor to VDD, thinking that should be enough. I had not placed the 2 pin header to connect it to ground yet. But after I soldered in the header and placed a jumper (pulling the BOOT0 pin to ground), the error no longer appeared and I was able to program, debug, trace through a program, and run it without a problem, using pretty much the default debugger config settings. Hope that helps!
2024-03-18 6:21 AM
Erase flash memory from cubeProgrammer and flash again my firmware from CubeIDE worked for me :thumbs_up: