cancel
Showing results for 
Search instead for 
Did you mean: 

How can I determine the starting address of the stack in CubeIDE?

DK.7
Senior

In Keil, if you open a file with the extension .map, you can find information about starting address of stack and so on. See screen.

How can I determine the starting address of the stack in CubeIDE?Q.png

1 ACCEPTED SOLUTION

Accepted Solutions

It should really use the space allocated by the linker, in this case ST just lets it descend into the end of the heap

See _sbrk implementation in syscalls.c

ST sets in to the end of RAM, and it auto-decrements from there, basically the first 32-bit word gets stored at _estack-4

_bstack = (ORIGIN (RAM) + LENGTH (RAM) - _Min_Stack_Size)

_estack = (ORIGIN (RAM) + LENGTH (RAM))

 

In the Keil builds the initial stack is set to __initial_sp, and descends too Stack_Mem

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

6 REPLIES 6
SofLit
ST Employee

Hello,

Go to STM32CubeIDE\Debug and open .map file. Try to find the line

_estack = (ORIGIN (RAM) + LENGTH (RAM))

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thanks for the answer!

I found the desired line in .map file

 

_estack = (ORIGIN (RAM) + LENGTH (RAM))

 

and I don’t understand what to do with it. See screen.Q.png

SofLit
ST Employee

 

SofLit_1-1706284458542.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thank you, but how to find out the end address of stack from this file?

SofLit
ST Employee

_estack defines the end of the Stack which is the Top of the stack.

So normally the stack starts at: _estack - _Min_Stack_Size

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

It should really use the space allocated by the linker, in this case ST just lets it descend into the end of the heap

See _sbrk implementation in syscalls.c

ST sets in to the end of RAM, and it auto-decrements from there, basically the first 32-bit word gets stored at _estack-4

_bstack = (ORIGIN (RAM) + LENGTH (RAM) - _Min_Stack_Size)

_estack = (ORIGIN (RAM) + LENGTH (RAM))

 

In the Keil builds the initial stack is set to __initial_sp, and descends too Stack_Mem

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..