cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, Has any one tried importing the 'voltage mode buck example project' as available for download here: www.biricha.com/ST-Discovery-Kit into the STMCube IDE?

vchilapu
Associate II

The reason I ask is, the application note 'an5496-buck-voltage-mode-with-the-bg474edpow1-discovery-kit-stmicroelectronics' says the Buck_VoltageMode_SW.ioc is setup to be used with IAR workbench. However the same application note also mentions 'STM Cube IDE' is compatible. But I am not successful in building the project with 'STMCube IDE'. Is there is a document that can help me with configuration part for the same.

0 REPLIES 0