cancel
Showing results for 
Search instead for 
Did you mean: 

haw to stm32-mw-openbl

Elmofty
Associate II

hello to all

i want to build project on bluepill board i want to include stm32-mw-openbl

i got it from https://github.com/STMicroelectronics/stm32-mw-openbl  is there any example for this

haw to include in ide

6 REPLIES 6
Peter BENSCH
ST Employee

Well, that is already the example you want.

However, you want to use a Blue Pill, which has been known for years to use illegal fakes instead of the original STM32F103, which work differently or not at all for a number of functions. I would therefore strongly recommend that you use a board with an original STM32, e.g. one of the universally usable NUCLEO boards.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Evangelist III

@Elmofty wrote:

i got it from https://github.com/STMicroelectronics/stm32-mw-openbl  


So you saw this:

 AndrewNeil_0-1707916720543.png 

and this:

 AndrewNeil_1-1707916778500.png 

 

Elmofty
Associate II

thanks for your replay i try to creat new project with device stm32f103c8t6 but haw to enable 

bootloader as https://github.com/STMicroelectronics/stm32-mw-openbl  in the mediaware which packet need to install

Did you read the "How to use" section?

Have you followed the videos ?

Elmofty
Associate II

i think there is miss understand i want to build a project to work as programmer i want to program stm23 device using the boot loader usart with another stm32f103 i means to make one device as programmer as host to connect to the another stm32f103 to program i have see the document an3155 and see all the command all i am looking for it there any lib i can use to build the host device

 

Well, that does sound like a completely different question to your original post!

You've marked this thread as solved - you need to undo that, or people will just assume that no further replies are needed!