2021-07-02 11:33 AM
How to generate a break when the supply voltage drops below a certain value in the HAL?
Andrzej
Solved! Go to Solution.
2021-07-20 8:58 AM
Generally one would pre-erase a sector, and then journal across it.
How long exactly is it taking now?
Is there some RTC, BKP or NVRAM you can use instead? Perhaps save data there, and go into STANDBY, save the FLASH when power restored.
Perhaps you can immediately gear-down to a slower clock to save power?
Have code in the IRQ Handler directly, and disable all other IRQs?
2021-07-02 11:41 AM
If the answers to your previous posts on this topic were insufficient, please reply there with further details rather than creating another duplicate post with the same question.
https://community.st.com/s/question/0D53W00000uYj4KSAS/stm32f746gdiscovery-pwrpvd-stm32cubeide
2021-07-02 11:52 AM
Hello @Andrzej Dębski ,
If by generating a break you mean resetting the microcontroller, please check the Power Supply Supervisor section (2.4) of the Reference manual.
In this case you should use not HAL but LL (stm32h7xx_ll_pwr.c) to access the registers.
Best regards,
@SBEN .2
2021-07-03 3:02 AM
I will follow the comments.
I am working on writing to a FLASH uint32_t variable, on power off. I am trying to do this using PVD. So far, no luck. I wrote to FLASH and blocked contact with the Discovery disc. Turning off the power and trying to connect to the programmer will not work.
Andrzej
2021-07-03 10:25 AM
I was able to program the break when the voltage dropped. I used the wrong instruction.
static void PVD_NVIC_Init(void) {
PWR_PVDTypeDef sConfigPVD;
sConfigPVD.PVDLevel = PWR_PVDLEVEL_6;
sConfigPVD.Mode = PWR_PVD_MODE_IT_FALLING;
HAL_PWR_ConfigPVD(&sConfigPVD);
HAL_PWR_EnablePVD();
}
Without interruption.
Now I will try to write to FLASH. I will inform.
Best regards
Andrzej
2021-07-03 11:50 AM
Writing flash into a collapsing supply, probably a good way to brick things.
2021-07-05 12:42 AM
I don't understand "brick". Please explain.. This is jargon?
regerds
Andrzej
2021-07-20 8:45 AM
I did the power-off memorization as shown. HAL_PWR_PVD and HAL_FLASH_Program interrupt.
void HAL_PWR_PVDCallback(void) {
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, ADD_FLASH, total_time)
== HAL_OK)
HAL_FLASH_Lock();
}Can you even speed up your programming?
Andrzej
2021-07-20 8:58 AM
Generally one would pre-erase a sector, and then journal across it.
How long exactly is it taking now?
Is there some RTC, BKP or NVRAM you can use instead? Perhaps save data there, and go into STANDBY, save the FLASH when power restored.
Perhaps you can immediately gear-down to a slower clock to save power?
Have code in the IRQ Handler directly, and disable all other IRQs?
2021-07-20 9:07 AM
I'll check how long it takes now. As a last resort, I will lower the clock. Obviously it works and I'm happy but I wonder if it wouldn't be enough.
Andrzej