Skip to main content
ADębs.1
Senior
Jun 29, 2021 1:38 PM UTC
Question

STM32F746GDISCOVERY, PWR_PVD, STM32CubeIDE

I want to make an interrupt when power > 2.0V.

STM32CubeIDE generated:

/**
 * @brief NVIC Configuration.
 * @retval None
 */
static void MX_NVIC_Init(void)
{
 /* PVD_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(PVD_IRQn, 8, 0);
 HAL_NVIC_EnableIRQ(PVD_IRQn);
 /* TIM3_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(TIM3_IRQn, 5, 0);
 HAL_NVIC_EnableIRQ(TIM3_IRQn);
 /* LTDC_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(LTDC_IRQn, 5, 0);
 HAL_NVIC_EnableIRQ(LTDC_IRQn);
}
 
/**
 * @brief CRC Initialization Function
 * @param None
 * @retval None
 */

Configuration:

 /* USER CODE BEGIN SysInit */

 PWR_PVDTypeDef sConfigPVD;

  sConfigPVD.PVDLevel = PWR_PVDLEVEL_0;

  sConfigPVD.Mode = PWR_PVD_MODE_IT_RISING;

  HAL_PWR_ConfigPVD(&sConfigPVD);

  HAL_PWR_EnablePVD();

 /* USER CODE END SysInit */

Initialize:

 /* Initialize interrupts */

 MX_NVIC_Init();

How and where to call an interrupt so that it sets the variable on = 0?

Andrzej

This topic has been closed for replies.