Skip to main content
ADębs.1
Senior
Jun 12, 2021 12:00 PM UTC
Solved

STM32F746G-DISCO, STM32CubeIDE, FLASH, supply voltage drop

Hi

How to generate an interrupt when the supply voltage drops?

Andrzej

This topic has been closed for replies.
TDK
TDKBest answer
Jun 16, 2021 1:26 PM UTC

5 replies

TDK
Jun 12, 2021 12:47 PM UTC

There are some predefined possibilities available with the PVD functionality.

For an arbitrary level, hook up an ADC to the supply (with resistor divider), or use the VBAT tap if VBAT=VDD, and use the ADC analog watchdog functionality.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ADębs.1
ADębs.1Author
Senior
Jun 16, 2021 9:44 AM UTC

I have the following:

/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
	if (GPIO_Pin == WE_Pin) {
		on = 1;
		HAL_FLASH_Unlock();
//		FLASH_Erase_Sector(FLASH_SECTOR_7, FLASH_VOLTAGE_RANGE_3);
		HAL_FLASHEx_Erase(FLASH_SECTOR_7, FLASH_VOLTAGE_RANGE_3);
		HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, FLASH_SECTOR_7, 400);
		HAL_FLASH_Lock();
		set_time = *(__uint32_t*) FLASH_SECTOR_7;
	}
}
/* USER CODE END 4 */

Why is it crashing on deleting FLASH?

greetings

Andrzej

TDK
TDKBest answer
Jun 16, 2021 1:26 PM UTC
ADębs.1
ADębs.1Author
Senior
Jul 5, 2021 4:03 PM UTC

1. I interrupted lowering the PVD below 3.0. Works.

2. I have set FLASH_EraseInitTypeDef EraseInitStruct;

void FLASH_Erase(void) {
	EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
	EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;
	EraseInitStruct.Sector = FLASH_SECTOR_7;
	EraseInitStruct.NbSectors = 1;
 
	HAL_FLASH_Unlock();
	if (HAL_FLASHEx_Erase(&EraseInitStruct, &SECTORError) != HAL_OK)
	;
}

3. I have inserted a FLASH record into the interrupt

void HAL_PWR_PVDCallback(void) {
 HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, FLASH_SECTOR_7, total_time);
	HAL_FLASH_Lock();
}

4. Builds without error

5. I have concerns about entering the program into DISCOVERY because I blocked the contact between DISCOVERY and Laptop when I entered it earlier.

6. is this program correct?

Other problem:

1. FLASH_SECTOR_7 has the address 0x08C0 0000

2. The IDE reads FFFF FFFF at this address

3. There should be a variable uint32_t total_time at this address

4. In Live Expression I read 4101158945 and not FFFF FFFF

5. These are different values. Why?

greetings

Andrzej

Piranha
Principal III
Jun 16, 2021 3:07 PM UTC

And apparently compiler warnings are also for kids, not "the real guys"...