2024-03-16 4:47 PM
After updating to STM32CubeIDE 1.14, I can't program my custom boards or Nucleos. I have tested three Nucleos.
Debug probe STL-LINK GDB server -> fails. All custom boards and Nucleos give me the same error, as seen in the image below.
Debug probe OpenOCD -> works fine on all boards and Nucleos.
STM32CubeProgrammer works fine.
I have reinstalled all programs a couple of times, but I keep getting the same error.
Any ideas?
GDB commad line:
C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.100.202310302101\tools\bin\ST-LINK_gdbserver.exe -p 61234 -l 1 -d -s -cp C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.100.202311100844\tools\bin -m 0 -g
st-link_gdbserver_log.txt
[0.000] initConfigParams(): Configuration flags start
[0.000] initConfigParams(): external-init false
[0.000] initConfigParams(): pend-halt-timeout (null)
[0.000] initConfigParams(): halt false
[0.000] initConfigParams(): config-file ""
[0.000] initConfigParams(): persistent false
[0.000] initConfigParams(): +log-file "C:\Users\Gamarra\STM32CubeIDE\workspace_1.14.1\01_test_run\Debug\st-link_gdbserver_log.txt"
[0.001] initConfigParams(): +log-level 31
[0.001] initConfigParams(): +port-number 61234
[0.001] initConfigParams(): +verbose true
[0.001] initConfigParams(): refresh-delay 15
[0.001] initConfigParams(): +verify true
[0.001] initConfigParams(): +swd true
[0.001] initConfigParams(): swo-port 61234
[0.001] initConfigParams(): cpu-clock 8000000
[0.001] initConfigParams(): swo-clock-div 128
[0.001] initConfigParams(): initialize-reset false
[0.001] initConfigParams(): debuggers false
[0.001] initConfigParams(): serial-number ""
[0.001] initConfigParams(): +apid 0
[0.001] initConfigParams(): +attach true
[0.001] initConfigParams(): shared false
[0.001] initConfigParams(): erase-all false
[0.001] initConfigParams(): memory-map ""
[0.001] initConfigParams(): ext-memory-loaders false
[0.001] initConfigParams(): extload_init (null)
[0.001] initConfigParams(): extload (null)
[0.001] initConfigParams(): +stm32cubeprogrammer-path "C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.100.202311100844\tools\bin"
[0.001] initConfigParams(): temp-path ""
[0.001] initConfigParams(): preserve-temps false
[0.001] initConfigParams(): frequency 0
[0.001] initConfigParams(): licenses false
[0.001] initConfigParams(): ignore-rest false
[0.001] initConfigParams(): version false
[0.001] initConfigParams(): help false
[0.001] initConfigParams(): Configuration flags end
Solved! Go to Solution.
2024-05-01 11:37 AM
After reinstalling Windows 10, DGB Server is working again.
2024-03-16 4:59 PM
Try to create new debug configuration for STL-LINK GDB server, rather than reusing configurations created before update.
2024-03-16 4:59 PM - edited 2024-03-16 6:17 PM
By the way, I tried:
To use different reset modes, software, hardware...
Erase the UCs with the STM32CubeProgrammer, erase is off but keep getting the same error.
Update the firmware, the last version is successfully flashed but keep getting the same error.
2024-03-16 5:05 PM
Try to create new debug configuration, rather than reusing configurations created before update.
2024-03-16 6:14 PM - edited 2024-03-16 6:24 PM
Hi Pavel
I deleted the .elf file, a new one is created when start a new debug/run sesions, it is Ok or I should try something else? After that problem persist.
2024-03-17 1:21 AM
> Debug probe OpenOCD -> works fine on all boards and Nucleos.
So why not use this ? (I most times use OpenOCD .)
+
> initConfigParams(): cpu-clock 800000
CPU is at 8M - really ?
see one of my settings with GDB:
2024-03-17 8:02 AM
@dhs Not the .elf file. Create a new debug configuration. Do not delete the old one yet, if you prefer.
2024-03-17 10:52 AM
Hi Pavel
I creted a new one and I still getting same error.
Open PCD workingfine , down the log:
Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
clock_config
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J13M4 (API v3) VID:PID 0483:3754
Info : Target voltage: 3.422163
Info : clock speed 8000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x0be12477
Info : [STM32U575VITxQ.cpu] Cortex-M33 r0p4 processor detected
Info : [STM32U575VITxQ.cpu] target has 8 breakpoints, 4 watchpoints
Info : gdb port disabled
Info : starting gdb server for STM32U575VITxQ.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : [STM32U575VITxQ.cpu] external reset detected
Info : accepting 'gdb' connection on tcp/3333
CPU in Non-Secure state
[STM32U575VITxQ.cpu] halted due to debug-request, current mode: Thread
xPSR: 0xf9000000 pc: 0x0800200c msp: 0x200c0000
STM32U575VITxQ.cpu TrustZone disabled
STM32U575VITxQ.cpu work-area address is set to 0x20000000
Info : device idcode = 0x20016482 (STM32U57/U58xx - Rev X : 0x2001)
Info : TZEN = 0 : TrustZone disabled by option bytes
Info : RDP level 0 (0xAA)
Info : flash size = 2048 KiB
Info : flash mode : dual-bank
Info : device idcode = 0x20016482 (STM32U57/U58xx - Rev X : 0x2001)
Info : TZEN = 0 : TrustZone disabled by option bytes
Info : RDP level 0 (0xAA)
Info : flash size = 2048 KiB
Info : flash mode : dual-bank
Info : device idcode = 0x20016482 (STM32U57/U58xx - Rev X : 0x2001)
Info : TZEN = 0 : TrustZone disabled by option bytes
Info : RDP level 0 (0xAA)
Info : OTP size is 512 bytes, base address is 0x0bfa0000
Info : New GDB Connection: 1, Target STM32U575VITxQ.cpu, state: halted
Info : accepting 'gdb' connection on tcp/3333
Info : New GDB Connection: 2, Target STM32U575VITxQ.cpu, state: halted
[STM32U575VITxQ.cpu] halted due to debug-request, current mode: Thread
xPSR: 0xf9000000 pc: 0x0800200c msp: 0x200c0000
Info : Padding image section 0 at 0x0800ce2c with 4 bytes (bank write end alignment)
[STM32U575VITxQ.cpu] halted due to debug-request, current mode: Thread
xPSR: 0xf9000000 pc: 0x0800200c msp: 0x200c0000
Info : dropped 'gdb' connection
[STM32U575VITxQ.cpu] halted due to debug-request, current mode: Thread
xPSR: 0x29000000 pc: 0x08002190 msp: 0x200bffc8
shutdown command invoked
Info : dropped 'gdb' connection
2024-03-18 2:31 PM
Then keep using the OpenOCD backend? Sorry, I'm of ideas ((
2024-03-18 3:37 PM
Currently I am using the OpenOCD, I tested same proyect, sames boards in other PCs, and GDB is ok, I am out of ideas too.