2024-03-16 4:47 PM
After updating to STM32CubeIDE 1.14, I can't program my custom boards or Nucleos. I have tested three Nucleos.
Debug probe STL-LINK GDB server -> fails. All custom boards and Nucleos give me the same error, as seen in the image below.
Debug probe OpenOCD -> works fine on all boards and Nucleos.
STM32CubeProgrammer works fine.
I have reinstalled all programs a couple of times, but I keep getting the same error.
Any ideas?
GDB commad line:
C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.100.202310302101\tools\bin\ST-LINK_gdbserver.exe -p 61234 -l 1 -d -s -cp C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.100.202311100844\tools\bin -m 0 -g
st-link_gdbserver_log.txt
[0.000] initConfigParams(): Configuration flags start
[0.000] initConfigParams(): external-init false
[0.000] initConfigParams(): pend-halt-timeout (null)
[0.000] initConfigParams(): halt false
[0.000] initConfigParams(): config-file ""
[0.000] initConfigParams(): persistent false
[0.000] initConfigParams(): +log-file "C:\Users\Gamarra\STM32CubeIDE\workspace_1.14.1\01_test_run\Debug\st-link_gdbserver_log.txt"
[0.001] initConfigParams(): +log-level 31
[0.001] initConfigParams(): +port-number 61234
[0.001] initConfigParams(): +verbose true
[0.001] initConfigParams(): refresh-delay 15
[0.001] initConfigParams(): +verify true
[0.001] initConfigParams(): +swd true
[0.001] initConfigParams(): swo-port 61234
[0.001] initConfigParams(): cpu-clock 8000000
[0.001] initConfigParams(): swo-clock-div 128
[0.001] initConfigParams(): initialize-reset false
[0.001] initConfigParams(): debuggers false
[0.001] initConfigParams(): serial-number ""
[0.001] initConfigParams(): +apid 0
[0.001] initConfigParams(): +attach true
[0.001] initConfigParams(): shared false
[0.001] initConfigParams(): erase-all false
[0.001] initConfigParams(): memory-map ""
[0.001] initConfigParams(): ext-memory-loaders false
[0.001] initConfigParams(): extload_init (null)
[0.001] initConfigParams(): extload (null)
[0.001] initConfigParams(): +stm32cubeprogrammer-path "C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.100.202311100844\tools\bin"
[0.001] initConfigParams(): temp-path ""
[0.001] initConfigParams(): preserve-temps false
[0.001] initConfigParams(): frequency 0
[0.001] initConfigParams(): licenses false
[0.001] initConfigParams(): ignore-rest false
[0.001] initConfigParams(): version false
[0.001] initConfigParams(): help false
[0.001] initConfigParams(): Configuration flags end
Solved! Go to Solution.
2024-05-01 11:37 AM
After reinstalling Windows 10, DGB Server is working again.