cancel
Showing results for 
Search instead for 
Did you mean: 

Fault analyzer toolbar missing

lucius92
Associate

Hello everybody,

Since I did last update of STM32CubeIDE software I cannot see the fault analyzer toolbar anymore (attached file img).

Am I missing some configuration to display it?

Or is due to the update?

Thank you for your time

 

5 REPLIES 5
Mahmoud Ben Romdhane
ST Employee

Hello @lucius92 ,

First let me thank you for posting and welcome to ST Community.

I suggest that you Select the menu command [Window]>[Show View]>[Others] and tap [Fault Analyzer] or use the [Quick Access] field and search for “Fault Analyzer” and select it from the views.

Thanks.

Mahmoud.

lucius92
Associate

Hello @Mahmoud Ben Romdhane 

I correctly display Fault analyzer but there is no toolbar  (also when there is a fault)

Cattura1.JPG

Hi Mahmoud,

I am seeing the same issue using the latest version. 

Dan

 

 

 

Hello,

 

The issue is reported internally to our team (Internal ticket number : 174586) and it will be fixed as soon as possible.

 

Thanks.

Mahmoud.

RobNewbury
Associate II

Did this issue get fixed?

I don't see the Fault Analyzer toolbar in the Fault Analyzer Window or am I just looking in the wrong place for it?

I'm using STM32CubeIDE V1.15.1 (Build 21094_20240412_1041)

TRobNewbury_0-1716365769736.png