2023-12-20 12:32 AM
Hello everybody,
Since I did last update of STM32CubeIDE software I cannot see the fault analyzer toolbar anymore (attached file img).
Am I missing some configuration to display it?
Or is due to the update?
Thank you for your time
Solved! Go to Solution.
2024-02-26 01:45 AM
Hello,
The issue is reported internally to our team (Internal ticket number : 174586) and it will be fixed as soon as possible.
Thanks.
Mahmoud.
2023-12-20 01:37 AM
Hello @lucius92 ,
First let me thank you for posting and welcome to ST Community.
I suggest that you Select the menu command [Window]>[Show View]>[Others] and tap [Fault Analyzer] or use the [Quick Access] field and search for “Fault Analyzer” and select it from the views.
Thanks.
Mahmoud.
2023-12-20 01:48 AM
Hello @Mahmoud Ben Romdhane
I correctly display Fault analyzer but there is no toolbar (also when there is a fault)
2024-02-24 10:33 PM
Hi Mahmoud,
I am seeing the same issue using the latest version.
Dan
2024-02-26 01:45 AM
Hello,
The issue is reported internally to our team (Internal ticket number : 174586) and it will be fixed as soon as possible.
Thanks.
Mahmoud.
2024-05-22 01:20 AM
Did this issue get fixed?
I don't see the Fault Analyzer toolbar in the Fault Analyzer Window or am I just looking in the wrong place for it?
I'm using STM32CubeIDE V1.15.1 (Build 21094_20240412_1041)
T