cancel
Showing results for 
Search instead for 
Did you mean: 

Errror while generating the code with STCube IDE

Shyam1
Associate II

Hi,

I am unable to generate the code with STcubeIDE for STM32H747I, will any one help me to sort this issue.

Version Details:

STcubeIDE : 1.13.1

CubeMX: 6.9.1

The error message is attached below

Error Msg.PNG

6 REPLIES 6
TDK
Guru

Open your IOC file, go to Project Manager and look at what firmware package it wants to use:

TDK_0-1692276727459.png

 

Then go to help -> Manage embedded software packages and download that package.

TDK_1-1692276770631.png

 

 

If you feel a post has answered your question, please click "Accept as Solution".
Shyam1
Associate II

Hi TDK,

I confirmed that the relevant package is installed, and in the CubeMX it is showing as available.

Is there any other check?

Hi @Shyam1 

Thank you for posting!

please check the connection (Preference>STM32Cube>Firmware updater) 

Capturze.PNG

Regards

Souhaib

 

Hi Souhaib,

Thanks for your support.

I tried with check connection, and could observe the same message see in the recommendation window. 

I have ensure it is up to date "Target Selector Device Database Updates"; and ensured the software packages is available in the repository.

 

Will you please help any other alternative....

 

 

Hi @Shyam1 

Are you using a proxy connection?

if yes please refer to this link How to set up proxy and P2P Ethernet connection with STM32CubeIDE - stm32mpu to set up your proxy connection with STM32CubeIDE.

thanks

Çözüm nedir. Bende de aynı hata var. Her şeyi denedim, çözülmedi