cancel
Showing results for 
Search instead for 
Did you mean: 

Errror while generating the code with STCube IDE

Shyam1
Associate II

Hi,

I am unable to generate the code with STcubeIDE for STM32H747I, will any one help me to sort this issue.

Version Details:

STcubeIDE : 1.13.1

CubeMX: 6.9.1

The error message is attached below

Error Msg.PNG

 

6 REPLIES 6
TDK
Super User

Open your IOC file, go to Project Manager and look at what firmware package it wants to use:

TDK_0-1692276727459.png

 

Then go to help -> Manage embedded software packages and download that package.

TDK_1-1692276770631.png

 

 

If you feel a post has answered your question, please click "Accept as Solution".
Shyam1
Associate II

Hi TDK,

I confirmed that the relevant package is installed, and in the CubeMX it is showing as available.

Is there any other check?

Hi @Shyam1 

Thank you for posting!

please check the connection (Preference>STM32Cube>Firmware updater) 

Capturze.PNG

Regards

Souhaib

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Souhaib,

Thanks for your support.

I tried with check connection, and could observe the same message see in the recommendation window. 

I have ensure it is up to date "Target Selector Device Database Updates"; and ensured the software packages is available in the repository.

 

Will you please help any other alternative....

 

 

Hi @Shyam1 

Are you using a proxy connection?

if yes please refer to this link How to set up proxy and P2P Ethernet connection with STM32CubeIDE - stm32mpu to set up your proxy connection with STM32CubeIDE.

thanks

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Çözüm nedir. Bende de aynı hata var. Her şeyi denedim, çözülmedi