cancel
Showing results for 
Search instead for 
Did you mean: 

embbeded stm32f746 nucleo board ethernet use

Snehal2001
Associate

stm32 nucleo board use ethernet communiction  send string on board pb7 led on same off string

 

It looks like you're trying to implement a TCP client on an STM32 Nucleo board that controls an LED connected to pin PB7 based on the string send  on  sever received from a TCP client. You mentioned that the code is not functioning as expected, specifically that the LED does not turn ON or OFF despite receiving the correct strings ("ON" or "OFF") from the Hercules TCP server. hercules software use 

3 REPLIES 3

@Snehal2001 wrote:

It looks like you're trying to ... 


Who are you addressing here? Is this meant to be a reply to something?

stm32 nucleo board use ethernet communiction  send string on board pb7 led on same off string

 

 

stm32f746 nucleo board use ethernet communiction herculus software use tcp server send string on tcp client receive string than board pb7 led on same off string ethernet use all file code send

 

 

That doesn't answer the question!

What are you talking about?

Do you have a question to ask?