2024-10-04 7:43 AM
Why am I getting 2 different fonts in these Memory views?
If I now create a new view, it uses a different font:
It seems that it only happens in a newly-created view; if I switch from that last one to one of the earlier views, then switch back again, it's changed font to the same as the earlier 2:
2024-10-07 7:23 AM
Hello @Andrew Neil
First let me thank you for posting.
I made the test but I was not able to see the same behavior.
I made the test with STM32CubeIDE 1.16.1 on a Windows 10 machine.
Are you using the similar setup?
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-07 7:59 AM
I'm using CubeIDE v1.13.0 on Win 11
Note that it only happens immediately the view is created.