2024-04-30 11:15 PM - edited 2024-04-30 11:53 PM
I am using Mac Os
I installed Cube IDE Version: 1.15.1. And tried to progarm ,i lost a lot of time by software error.
When i configure the .ioc where I configured TIM1 with some parameter .
After the code generated and wrote some programs ,but not worked, the problem the .ioc auto generate didnt generated the __HAL_RCC_GPIOB_CLK_ENABLE(); is it normally or any other problem with me ?
so the TIM will not turn on
.
Also there are another problem i found is
In new project ,we trying to enter the stm32 controller to enter the selector only one letter is pressing and the next entry is automatically jumped to the next entry field ,irritating . pleas correct it ,
Whcih one is the stable version ?
2024-05-02 09:14 AM
Hello @thannara123,
>>When i configure the .ioc where I configured TIM1 with some parameter
Could you specify more the TIM config or provide a minimal code so we can reproduce it on our side?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-03 01:01 AM
Hi TImer configuration was corrected mistaken by some calculation . Some of time when i generate the configuration to code it actually not generate all ,we need to repate the code generation ?
And also please make solution for In new project ,we trying to enter the stm32 controller to enter the selector only one letter is pressing and the next entry is automatically jumped to the next entry field
2024-05-09 02:23 AM
Hello @thannara123
I reported the part number issue internally for further investigation.
Internal ticket number: 180961 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.