cancel
Showing results for 
Search instead for 
Did you mean: 

Cube IDE: Running, and being able to reset and re-run, a program from 0x8008000 (ie offset from where a bootloader would live)

DiBosco
Senior II

If I have a bootloader that resides at 0x8000000 and the main program starts at 0x8008000 I can load it with the debugger and all is fine. I can run it in standa alone mode with the bootloader jumping to it as well. However, if I try to restart and rerun the program with the debugger it doesn't work and I have to reprogram. Is there a way to set up the debugger so that I don't have reprogram each time please?

FWIW doing this on a L476.

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
DiBosco
Senior II

Hi, thanks for the reply. I should really have said that I'd already tried that to no avail.

A colleague came up with the idea of putting;

set $pc=Reset_Handler

In Restart Configurations. That seems to work and is surprisingly, not ephemeral.

View solution in original post

3 REPLIES 3
Guillaume K
ST Employee

Hello

In STM32CubeIDE 1.7.0, when you create a debug configuration for "STM32 Cortex-M C/C++ Application" there is a Startup tab. In "Runtime options": try to set start address 0x08008000 in "Set program counter (hex) :" or "Specify vector table (hex):" (if you have moved the Interrupt vector table to 0x08008000).

DiBosco
Senior II

Hi, thanks for the reply. I should really have said that I'd already tried that to no avail.

A colleague came up with the idea of putting;

set $pc=Reset_Handler

In Restart Configurations. That seems to work and is surprisingly, not ephemeral.

Thanks!  I had the same problem and it had me discouraged for about a week.  This seems to have fixed it right away.