cancel
Showing results for 
Search instead for 
Did you mean: 

Cube IDE 1.15.1 - FreeRTOS Debugger view - List Task Window - name of task issue

antweb
Associate II

Hello everyone,

I have issue with showing up names of tasks in the FreeRTOS Task List window during debugging. I have attached screen of the current issue. As we can see there are two tasks with incorrect names (only the first letter of each task is displaying). 

Did anyone have a similar problem?

 

8 REPLIES 8
Souhaib MAZHOUD
ST Employee

Hello @antweb 

Thank you for posting!

Could you please provide your .ioc file in order to investigate the issue.

BR,

Souhaib

antweb
Associate II

Hello @Souhaib MAZHOUD 
Of course, below is the .ioc file content (also I've attached the file):

 

#MicroXplorer Configuration settings - do not modify CAD.formats=[] CAD.pinconfig=Dual CAD.provider= ETH.IPParameters=MediaInterface ETH.MediaInterface=HAL_ETH_RMII_MODE FREERTOS.IPParameters=Tasks01,configUSE_NEWLIB_REENTRANT FREERTOS.Tasks01=defaultTask,24,128,StartDefaultTask,Default,NULL,Dynamic,NULL,NULL FREERTOS.configUSE_NEWLIB_REENTRANT=1 File.Version=6 GPIO.groupedBy=Group By Peripherals KeepUserPlacement=false LWIP.BSP.number=1 LWIP.ETHARP_DEBUG=LWIP_DBG_ON LWIP.GATEWAY_ADDRESS=192.168.000.001 LWIP.HTTPD_DEBUG=LWIP_DBG_ON LWIP.IPParameters=LWIP_DHCP,IP_ADDRESS,NETMASK_ADDRESS,GATEWAY_ADDRESS,MEM_SIZE,ETHARP_DEBUG,NETIF_DEBUG,HTTPD_DEBUG,LWIP_STATS,LWIP_STATS_DISPLAY,LINK_STATS LWIP.IP_ADDRESS=192.168.000.222 LWIP.LINK_STATS=1 LWIP.LWIP_DHCP=0 LWIP.LWIP_STATS=1 LWIP.LWIP_STATS_DISPLAY=1 LWIP.MEM_SIZE=10*1024 LWIP.NETIF_DEBUG=LWIP_DBG_ON LWIP.NETMASK_ADDRESS=255.255.255.000 LWIP.Version=v2.1.2_Cube LWIP0.BSP.STBoard=false LWIP0.BSP.api=BSP_COMPONENT_DRIVER LWIP0.BSP.component=LAN8742 LWIP0.BSP.condition= LWIP0.BSP.instance=LAN8742 LWIP0.BSP.ip= LWIP0.BSP.mode= LWIP0.BSP.name=Driver_PHY LWIP0.BSP.semaphore=S_LAN8742 LWIP0.BSP.solution=LAN8742 Mcu.CPN=STM32F439ZIT6 Mcu.Family=STM32F4 Mcu.IP0=ETH Mcu.IP1=FREERTOS Mcu.IP2=LWIP Mcu.IP3=NVIC Mcu.IP4=RCC Mcu.IP5=SYS Mcu.IP6=USART3 Mcu.IPNb=7 Mcu.Name=STM32F439Z(G-I)Tx Mcu.Package=LQFP144 Mcu.Pin0=PH0/OSC_IN Mcu.Pin1=PH1/OSC_OUT Mcu.Pin10=PB13 Mcu.Pin11=PD8 Mcu.Pin12=PD9 Mcu.Pin13=PD3 Mcu.Pin14=VP_FREERTOS_VS_CMSIS_V2 Mcu.Pin15=VP_LWIP_VS_Enabled Mcu.Pin16=VP_SYS_VS_tim3 Mcu.Pin2=PC1 Mcu.Pin3=PA1 Mcu.Pin4=PA2 Mcu.Pin5=PA7 Mcu.Pin6=PC4 Mcu.Pin7=PC5 Mcu.Pin8=PB11 Mcu.Pin9=PB12 Mcu.PinsNb=17 Mcu.ThirdPartyNb=0 Mcu.UserConstants= Mcu.UserName=STM32F439ZITx MxCube.Version=6.11.1 MxDb.Version=DB.6.0.111 NVIC.BusFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false NVIC.DebugMonitor_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false NVIC.ETH_IRQn=true\:5\:0\:false\:false\:true\:true\:true\:true\:true NVIC.ForceEnableDMAVector=true NVIC.HardFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false NVIC.MemoryManagement_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false NVIC.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false NVIC.PendSV_IRQn=true\:15\:0\:false\:false\:false\:true\:false\:false\:false NVIC.PriorityGroup=NVIC_PRIORITYGROUP_4 NVIC.SVCall_IRQn=true\:0\:0\:false\:false\:false\:false\:false\:false\:false NVIC.SavedPendsvIrqHandlerGenerated=true NVIC.SavedSvcallIrqHandlerGenerated=true NVIC.SavedSystickIrqHandlerGenerated=true NVIC.SysTick_IRQn=true\:15\:0\:false\:false\:false\:true\:false\:true\:false NVIC.TIM3_IRQn=true\:15\:0\:false\:false\:true\:false\:false\:true\:true NVIC.TimeBase=TIM3_IRQn NVIC.TimeBaseIP=TIM3 NVIC.UsageFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false PA1.Mode=RMII PA1.Signal=ETH_REF_CLK PA2.Mode=RMII PA2.Signal=ETH_MDIO PA7.Mode=RMII PA7.Signal=ETH_CRS_DV PB11.Mode=RMII PB11.Signal=ETH_TX_EN PB12.Mode=RMII PB12.Signal=ETH_TXD0 PB13.Mode=RMII PB13.Signal=ETH_TXD1 PC1.Mode=RMII PC1.Signal=ETH_MDC PC4.Mode=RMII PC4.Signal=ETH_RXD0 PC5.Mode=RMII PC5.Signal=ETH_RXD1 PD3.GPIOParameters=PinState PD3.Locked=true PD3.PinState=GPIO_PIN_RESET PD3.Signal=GPIO_Output PD8.Locked=true PD8.Mode=Asynchronous PD8.Signal=USART3_TX PD9.Mode=Asynchronous PD9.Signal=USART3_RX PH0/OSC_IN.Mode=HSE-External-Oscillator PH0/OSC_IN.Signal=RCC_OSC_IN PH1/OSC_OUT.Mode=HSE-External-Oscillator PH1/OSC_OUT.Signal=RCC_OSC_OUT PinOutPanel.RotationAngle=0 ProjectManager.AskForMigrate=true ProjectManager.BackupPrevious=false ProjectManager.CompilerOptimize=6 ProjectManager.ComputerToolchain=false ProjectManager.CoupleFile=true ProjectManager.CustomerFirmwarePackage= ProjectManager.DefaultFWLocation=true ProjectManager.DeletePrevious=true ProjectManager.DeviceId=STM32F439ZITx ProjectManager.FirmwarePackage=STM32Cube FW_F4 V1.28.0 ProjectManager.FreePins=false ProjectManager.HalAssertFull=false ProjectManager.HeapSize=0x200 ProjectManager.KeepUserCode=true ProjectManager.LastFirmware=true ProjectManager.LibraryCopy=1 ProjectManager.MainLocation=Core/Src ProjectManager.NoMain=false ProjectManager.PreviousToolchain=STM32CubeIDE ProjectManager.ProjectBuild=false ProjectManager.ProjectFileName=IoT_F439.ioc ProjectManager.ProjectName=IoT_F439 ProjectManager.ProjectStructure= ProjectManager.RegisterCallBack= ProjectManager.StackSize=0x400 ProjectManager.TargetToolchain=STM32CubeIDE ProjectManager.ToolChainLocation= ProjectManager.UAScriptAfterPath= ProjectManager.UAScriptBeforePath= ProjectManager.UnderRoot=true ProjectManager.functionlistsort=1-SystemClock_Config-RCC-false-HAL-false,2-MX_GPIO_Init-GPIO-false-HAL-true,3-MX_USART3_UART_Init-USART3-false-HAL-true,4-MX_LWIP_Init-LWIP-false-HAL-false RCC.48MHZClocksFreq_Value=90000000 RCC.AHBFreq_Value=180000000 RCC.APB1CLKDivider=RCC_HCLK_DIV4 RCC.APB1Freq_Value=45000000 RCC.APB1TimFreq_Value=90000000 RCC.APB2CLKDivider=RCC_HCLK_DIV2 RCC.APB2Freq_Value=90000000 RCC.APB2TimFreq_Value=180000000 RCC.CortexFreq_Value=180000000 RCC.EthernetFreq_Value=180000000 RCC.FCLKCortexFreq_Value=180000000 RCC.FamilyName=M RCC.HCLKFreq_Value=180000000 RCC.HSE_VALUE=8000000 RCC.HSI_VALUE=16000000 RCC.I2SClocksFreq_Value=192000000 RCC.IPParameters=48MHZClocksFreq_Value,AHBFreq_Value,APB1CLKDivider,APB1Freq_Value,APB1TimFreq_Value,APB2CLKDivider,APB2Freq_Value,APB2TimFreq_Value,CortexFreq_Value,EthernetFreq_Value,FCLKCortexFreq_Value,FamilyName,HCLKFreq_Value,HSE_VALUE,HSI_VALUE,I2SClocksFreq_Value,LCDTFTFreq_Value,LSE_VALUE,LSI_VALUE,MCO2PinFreq_Value,PLLCLKFreq_Value,PLLM,PLLN,PLLQCLKFreq_Value,PLLSourceVirtual,RTCFreq_Value,RTCHSEDivFreq_Value,SAI_AClocksFreq_Value,SAI_BClocksFreq_Value,SYSCLKFreq_VALUE,SYSCLKSource,VCOI2SOutputFreq_Value,VCOInputFreq_Value,VCOOutputFreq_Value,VCOSAIOutputFreq_Value,VCOSAIOutputFreq_ValueQ,VCOSAIOutputFreq_ValueR,VcooutputI2S,VcooutputI2SQ RCC.LCDTFTFreq_Value=24500000 RCC.LSE_VALUE=32768 RCC.LSI_VALUE=32000 RCC.MCO2PinFreq_Value=180000000 RCC.PLLCLKFreq_Value=180000000 RCC.PLLM=4 RCC.PLLN=180 RCC.PLLQCLKFreq_Value=90000000 RCC.PLLSourceVirtual=RCC_PLLSOURCE_HSE RCC.RTCFreq_Value=32000 RCC.RTCHSEDivFreq_Value=4000000 RCC.SAI_AClocksFreq_Value=24500000 RCC.SAI_BClocksFreq_Value=24500000 RCC.SYSCLKFreq_VALUE=180000000 RCC.SYSCLKSource=RCC_SYSCLKSOURCE_PLLCLK RCC.VCOI2SOutputFreq_Value=384000000 RCC.VCOInputFreq_Value=2000000 RCC.VCOOutputFreq_Value=360000000 RCC.VCOSAIOutputFreq_Value=98000000 RCC.VCOSAIOutputFreq_ValueQ=24500000 RCC.VCOSAIOutputFreq_ValueR=49000000 RCC.VcooutputI2S=192000000 RCC.VcooutputI2SQ=192000000 USART3.IPParameters=VirtualMode USART3.VirtualMode=VM_ASYNC VP_FREERTOS_VS_CMSIS_V2.Mode=CMSIS_V2 VP_FREERTOS_VS_CMSIS_V2.Signal=FREERTOS_VS_CMSIS_V2 VP_LWIP_VS_Enabled.Mode=Enabled VP_LWIP_VS_Enabled.Signal=LWIP_VS_Enabled VP_SYS_VS_tim3.Mode=TIM3 VP_SYS_VS_tim3.Signal=SYS_VS_tim3 board=custom isbadioc=false
View more

 

 

Souhaib MAZHOUD
ST Employee

Hello @antweb 

Could you provide more information about the OS you using!

antweb
Associate II

Hello @Souhaib MAZHOUD 

I am using macOS Sonoma ver. 14.5 on MacBook Pro (chip: Apple M1 Pro).

Thank you @antweb

Actually, we are investigating this issue internally and I will keep you updated.

KR,

Souhaib

Curiouser and curiouser. I thought the problem was with ThreadX thread names, but FreeRTOS task names as well? And on a Mac again.

I will wait. Thx @Souhaib MAZHOUD 

Anything is know?