cancel
Showing results for 
Search instead for 
Did you mean: 

Could not determine GDB version

MikeMcCormack
Associate II

I am receiving this message 3 out of 4 times (approximately) after I just "upgraded" the IDE to 1.15.1 while using a Nucleo STM32H563 board.
Capture.PNG

 

My debugger config screen looks like

 

Capture2.PNG

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

By noticing this :

SofLit_0-1715263527750.png

This example is not available for H5 product. I have a doubt you're using a project not intended to be used for H5.

Could you please check?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Is the package downloaded from https://www.st.com/en/embedded-software/stm32cubeh5.html not meant for the STM32H5 family of parts?  My apologies.  I just assumed that since the path below

Capture4.PNG

literally contained the Nucleo board I was using that it was intended for that board.

 

BTW - how does the name of the project alter the GDB error I was receiving?  Can you tell me how I can fix the GDB problem or not, I'll be glad to change the project name or load another example if you prefer.

You're correct. 

Seems the board has that FDCAN examples that I'm not aware of :)!: https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H563ZI/Examples/FDCAN/FDCAN_Classic_Frame_Networking 

It have been added in newest version of the CubeH5. Was not available in V1.0.0. 

Meanwhile I didn't reproduce the issue on a Nucleo STM32H563 with STM32CubeIDE V1.15.1.

Did you update the STLINK firmware?

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Yes, following the upgrade to the IDE it indicated that there was newer firmware so I let it upgrade.  I have power cycled the board since then.