Channel 8 (and over) of DMA stream lead to code generation error on UART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-22 8:08 AM
Hello,
I use:
CubeIDE 1.3.0
STM32Cube_FW_F4_1.25.0
STM32F413CHU
I want to use DMA on UART5 on this uC but generated code does not compile.
Channel used by this UART is DMA1->Stream7->Channel8
I use LL, not HAL for UART.
Into MX_UART5_Init function (Core/Src/usart.c), called in main, there is this following line:
LL_DMA_SetChannelSelection(DMA1, LL_DMA_STREAM_7, DMA_CHANNEL_8);
Unfortunately,DMA_CHANNEL_8 is not defined.
Actually, DMA_CHANNEL_x are not defined. However LL_DMA_CHANNEL_1 to LL_DMA_CHANNEL_7 are defined.
I added LL_DMA_CHANNEL_8 (into Drivers/STM32F4xx_HAL_Driver/STM32F4xx_ll_dma.h):
#define LL_DMA_CHANNEL_8 DMA_SxCR_CHSEL_3
I replaced DMA_CHANNEL_8 to LL_DMA_CHANNEL_8 and my code is compiling.
My code generation produces an error.
Is it a bug?
Thanks for your help.
- Labels:
-
DMA
-
STM32CubeIDE
-
STM32F4 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-22 9:07 AM
Appears to be a bug/omission. They are defined within stm32f4xx_hal_dma.h but not within stm32f4xx_ll_dma.h.
#if defined (DMA_SxCR_CHSEL_3)
#define DMA_CHANNEL_8 0x10000000U /*!< DMA Channel 8 */
#define DMA_CHANNEL_9 0x12000000U /*!< DMA Channel 9 */
#define DMA_CHANNEL_10 0x14000000U /*!< DMA Channel 10 */
#define DMA_CHANNEL_11 0x16000000U /*!< DMA Channel 11 */
#define DMA_CHANNEL_12 0x18000000U /*!< DMA Channel 12 */
#define DMA_CHANNEL_13 0x1A000000U /*!< DMA Channel 13 */
#define DMA_CHANNEL_14 0x1C000000U /*!< DMA Channel 14 */
#define DMA_CHANNEL_15 0x1E000000U /*!< DMA Channel 15 */
#endif /* DMA_SxCR_CHSEL_3 */
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-22 9:19 AM
> I added LL_DMA_CHANNEL_8 (into Drivers/STM32F4xx_HAL_Driver/STM32F4xx_ll_dma.h):
> #define LL_DMA_CHANNEL_8 DMA_SxCR_CHSEL_3
#define DMA_SxCR_CHSEL_3 0x10000000U
#define DMA_CHANNEL_8 0x10000000U /*!< DMA Channel 8 */
To me, these look identical.
> My code generation produces an error.
What does this exactly mean?
Do you need to *generate* the code? Can't you simply compile and run it?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-25 3:44 AM
Thanks for your response.
I agree with you but in my project, CubeIDE produces:
#define DMA_SxCR_CHSEL_3 0x10000000U
(into stm32f413xx.h), but not:
#define DMA_CHANNEL_8 0x10000000U
DMA_CHANNEL_8 is not defined at all
That's why I have defined LL_DMA_CHANNEL_8 myself.
Therefore, I can't compile and run the code after CubeIDE code generation (using CubeMX).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-25 3:51 AM
Thanks for your help.
I will create a bug report using your answer.