2022-12-08 12:02 PM
Update: To get it to work, do a fresh install of the IDE, untick the CDT site in "Available Software Sites" (Help->Install New Software then "Manage"), and then install DevStyle from marketplace
Sister issue on the Genuitec forum site: https://www.genuitec.com/forums/topic/devstyle-not-installing-in-stm32cubeide/
I use STM32CubeIDE with the DevStyle Darkest Dark Theme extension from Eclipse Marketplace on two different 64-bit windows 10 computers without problem.
Over the past couple of days, I've been trying to install the same plugin on a different 64-bit windows 10 computer but it doesn't seem to work.
After a fresh install of STM32CubeIDE_v1.11.0_13638_20221122_1308, I do the following:
Then I leave the default components selected and I click on the Confirm button:
after processing the click for about 20 seconds, I get the following error displayed:
The installation cannot be completed as requested.
If I click Show original error and build my own solution radio button I get:
Here is the specific error message copy/pasted:
Cannot complete the install because one or more required items could not be found.
Software being installed: DevStyle with CodeTogether Bundle 1.11.0.202206271604 (com.genuitec.eclipse.theming.feature.feature.group 1.11.0.202206271604)
Missing requirement: DevStyle with CodeTogether Bundle 1.11.0.202206271604 (com.genuitec.eclipse.theming.feature.feature.group 1.11.0.202206271604) requires 'org.eclipse.equinox.p2.iu; com.genuitec.eclipse.codetogether.feature.feature.group 1.0.0' but it could not be found
If I then select "show original error and build my own solution" and select Install fewer items than originally requested then it appears to break the IDE because I can no longer build my project after the IDE restarts following the partial install
Does anyone else have this problem or know how to fix it?
Solved! Go to Solution.
2022-12-12 1:01 AM
Sorry to read this, and indeed I confirm that DevStyle breaks the IDE with default settings.
To get it working I had to do a fresh installation again, untick the CDT url from the Available Software Sites list, and install DevStyle again with only the required feature selected. Not straightforward I must admit (ticket logged internally).
2022-12-08 12:53 PM
2022-12-08 9:07 PM
What extras are you referring to?
If I select Keep me installation same and modify the items being installed to be compatible option then it does the same thing (i.e. DevStyle with CodeTogether Bundle will not be installed.
If I use the IDE without the darkest dark extension installed (or partially installed) then it works fine.
As mentioned above, this is working on two other computers with fresh windows 10 installs.
I tried a few different previous versions of the STM32Cube IDE but all encounter the same error on this particular PC.
2022-12-09 12:45 AM
Sometimes it helps for installations when CubeIDE is run as an administrator.
2022-12-09 5:27 AM
AFAIK the issue is about the DevStyle with CodeTogether Bundle feature. If you simply get the required feature selected then it should work.
For more details I encourage you to contact directly the software provider, see https://www.genuitec.com/products/devstyle/
2022-12-09 10:00 AM
2022-12-12 1:01 AM
Sorry to read this, and indeed I confirm that DevStyle breaks the IDE with default settings.
To get it working I had to do a fresh installation again, untick the CDT url from the Available Software Sites list, and install DevStyle again with only the required feature selected. Not straightforward I must admit (ticket logged internally).