cancel
Showing results for 
Search instead for 
Did you mean: 

Can't update Cube IDE

Dfarr.1
Senior

I cannot run updates from within Cube IDE.

Help>Check For Updates throws the following error dialog:

Unable to read repository at

https://sw-center.st.com/stm32cubeide/updatesite1/.

Unable to read repository at

http://sw-center.st.com/stm32cubeide/eclipse.

I have tried the following:

  • manually clear p2 cache and restart IDE
  • add https:// variant for the updatesite1
  • remove http:// variant for updatesite1
  • append "/" to the end of all Available software paths that don't have one.
  • remove and replace all Available Software Sites
  • export Available software paths from another PC without this issue, import into my PC.
  • launch the IDE from command line with stm32cubeide.exe -clean
  • reduce number of Available Software Sites to 2 only (eclipse repository, updatesite1)
  • Help>Install New Software : uncheck "contact all update sites during install to find required software"

None have worked.

I originally had 1.3.0 ide on my machine, it also could not be updated (checksum error that time). I manually downloaded and installed 1.4.0. But the update problem has persisted in this new form. I need to upgrade to 1.4.2 to collaborate with the rest of my team.

What else can I try?

1 ACCEPTED SOLUTION

Accepted Solutions
Julien D
ST Employee

Hi Dfarr.1

Thanks for reporting, there was an issue with the repository.

It should be fixed right now.

Could you reload every checked repository sites from Window > Preferences > Install/Update > Available Software Sites and try to update again (Help > Check for update) ?

Paste there any error which might occurs during the refresh.

View solution in original post

5 REPLIES 5
TDK
Guru

For what it's worth, I get the same error currently and my updates have worked in the past. It might be a transient issue that will get fixed if you just wait.

If you feel a post has answered your question, please click "Accept as Solution".
Julien D
ST Employee

Hi Dfarr.1

Thanks for reporting, there was an issue with the repository.

It should be fixed right now.

Could you reload every checked repository sites from Window > Preferences > Install/Update > Available Software Sites and try to update again (Help > Check for update) ?

Paste there any error which might occurs during the refresh.

Dfarr.1
Senior

Reload Available Software Sites successful.

First attempt at Check For Updates failed with a SHA256 error. I closed all projects, changed the updatesite1 address to https:// and added "/" on the end and ran again. It worked with those changes.

Thanks for the help.

Thank you! I have finally managed to update CubeIDE too using your suggestion.

I added a new Software Sites option starting with https:// then unticked all the others and it worked just fine. Should I re-tick any of the other options?

On a related note, do you also update the Eclipse CDT from the Eclipse Marketplace or is that not needed?

0693W00000Dm8hQQAR.png

Sorry @Community member​ , I'm not in a position to offer any further advice. I'm just an average user like yourself and I can really only vouch for my suggested solution, nothing more.