2020-11-02 2:39 PM
I cannot run updates from within Cube IDE.
Help>Check For Updates throws the following error dialog:
Unable to read repository at
https://sw-center.st.com/stm32cubeide/updatesite1/.
Unable to read repository at
http://sw-center.st.com/stm32cubeide/eclipse.
I have tried the following:
None have worked.
I originally had 1.3.0 ide on my machine, it also could not be updated (checksum error that time). I manually downloaded and installed 1.4.0. But the update problem has persisted in this new form. I need to upgrade to 1.4.2 to collaborate with the rest of my team.
What else can I try?
Solved! Go to Solution.
2020-11-02 11:34 PM
Hi Dfarr.1
Thanks for reporting, there was an issue with the repository.
It should be fixed right now.
Could you reload every checked repository sites from Window > Preferences > Install/Update > Available Software Sites and try to update again (Help > Check for update) ?
Paste there any error which might occurs during the refresh.
2020-11-02 4:32 PM
For what it's worth, I get the same error currently and my updates have worked in the past. It might be a transient issue that will get fixed if you just wait.
2020-11-02 11:34 PM
Hi Dfarr.1
Thanks for reporting, there was an issue with the repository.
It should be fixed right now.
Could you reload every checked repository sites from Window > Preferences > Install/Update > Available Software Sites and try to update again (Help > Check for update) ?
Paste there any error which might occurs during the refresh.
2020-11-03 8:55 AM
Reload Available Software Sites successful.
First attempt at Check For Updates failed with a SHA256 error. I closed all projects, changed the updatesite1 address to https:// and added "/" on the end and ran again. It worked with those changes.
Thanks for the help.
2021-09-03 9:51 AM
Thank you! I have finally managed to update CubeIDE too using your suggestion.
I added a new Software Sites option starting with https:// then unticked all the others and it worked just fine. Should I re-tick any of the other options?
On a related note, do you also update the Eclipse CDT from the Eclipse Marketplace or is that not needed?
2021-09-07 9:52 AM
Sorry @Community member , I'm not in a position to offer any further advice. I'm just an average user like yourself and I can really only vouch for my suggested solution, nothing more.