2023-06-21 12:56 AM
Hello,
I'm currently using stm32F410, i want to get to the system memory in order to use bootloader in UART and upgrade my firmware. I saw on datasheet that i need to pilot pin BOOT1. The problem is that on the graphical interface of STM32CubeIDE or CubeMx, when i click on PB2 (that should have the additionnal function "BOOT1"), i can't find BOOT1.
I saw that someone had a problem like this in 2018. I would like to know if it's fix or if there's another way to do it. I tried some otherm STM such as STM32F401 / F407, same problem. Only one card worked, it was the STM32F303 because i have to configure option bytes for BOOT1 and not pins.
Waiting for your responses.
Thanks.
Cyril.
Solved! Go to Solution.
2023-06-21 02:01 AM
The pin does not have to be specially configured as BOOT1, but is queried (sampled) exactly once with the fourth rising edge of SYSCLK after a reset. The schematics would therefore have to be designed in such a way that BOOT1 (PB2) can be set accordingly without significantly disturbing or even damaging the application.
Regards
/Peter
2023-06-21 01:08 AM - edited 2023-06-21 01:08 AM
This may indeed be confusing, however the RM0401, section 2.6 writes about it:
The values on the BOOT pins are latched on the 4th rising edge of SYSCLK after a reset. It
is up to the user to set the BOOT1 and BOOT0 pins after reset to select the required boot
mode.
BOOT0 is a dedicated pin while BOOT1 is shared with a GPIO pin. Once BOOT1 has been
sampled, the corresponding GPIO pin is free and can be used for other purposes.
Hope that helps?
Regards
/Peter
2023-06-21 01:21 AM
Thanks for responding that quick.
Actually, i don't know how to configure it when it doesn't appear on the GUI. What do you mean by sampling BOOT1 ?
Regards,
Cyril.
2023-06-21 02:01 AM
The pin does not have to be specially configured as BOOT1, but is queried (sampled) exactly once with the fourth rising edge of SYSCLK after a reset. The schematics would therefore have to be designed in such a way that BOOT1 (PB2) can be set accordingly without significantly disturbing or even damaging the application.
Regards
/Peter
2023-06-22 01:57 AM
It worked, thanks you, now i have to talk with my bootloader 🙂
2023-06-22 02:06 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter